# Copyright (C) 1991-2018 Free Software Foundation, Inc.
# This file is part of the GNU C Library.

# The GNU C Library is free software; you can redistribute it and/or
# modify it under the terms of the GNU Lesser General Public
# License as published by the Free Software Foundation; either
# version 2.1 of the License, or (at your option) any later version.

# The GNU C Library is distributed in the hope that it will be useful,
# but WITHOUT ANY WARRANTY; without even the implied warranty of
# MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
# Lesser General Public License for more details.

# You should have received a copy of the GNU Lesser General Public
# License along with the GNU C Library; if not, see
# <http://www.gnu.org/licenses/>.

#
#	Makefile for locales.
#
subdir	:= locale

include ../Makeconfig

headers		= langinfo.h locale.h bits/locale.h \
		  bits/types/locale_t.h bits/types/__locale_t.h
routines	= setlocale findlocale loadlocale loadarchive \
		  localeconv nl_langinfo nl_langinfo_l mb_cur_max \
		  newlocale duplocale freelocale uselocale \
		  catnames
tests		= tst-C-locale tst-locname tst-duplocale
categories	= ctype messages monetary numeric time paper name \
		  address telephone measurement identification collate
aux		= $(categories:%=lc-%) $(categories:%=C-%) SYS_libc C_name \
		  xlocale localename global-locale coll-lookup
others		= localedef locale
#others-static	= localedef locale
install-bin	= localedef locale
extra-objs	= $(localedef-modules:=.o) $(localedef-aux:=.o) \
		  $(locale-modules:=.o) $(lib-modules:=.o)

extra-libs	= libBrokenLocale
extra-libs-others = $(extra-libs)

libBrokenLocale-routines = broken_cur_max

subdir-dirs	= programs
vpath %.c programs ../crypt
vpath %.h programs
vpath %.gperf programs

localedef-modules	:= localedef $(categories:%=ld-%) \
			   charmap linereader locfile \
			   repertoire locarchive
localedef-aux		:= md5
locale-modules		:= locale locale-spec
lib-modules		:= charmap-dir simple-hash xmalloc xstrdup \
			   record-status


GPERF = gperf
GPERFFLAGS = -acCgopt -k1,2,5,9,$$ -L ANSI-C

include ../Rules

CFLAGS-md5.c += -I../crypt

programs/%-kw.h: programs/%-kw.gperf
	cd programs \
	&& $(GPERF) $(GPERFFLAGS) -N $(@F:-kw.h=_hash) $(<F) > $(@F).new
	mv -f $@.new $@

$(objpfx)localedef: $(localedef-modules:%=$(objpfx)%.o)
$(objpfx)localedef: $(localedef-aux:%=$(objpfx)%.o)
$(objpfx)locale: $(locale-modules:%=$(objpfx)%.o)
$(objpfx)localedef $(objpfx)locale: $(lib-modules:%=$(objpfx)%.o)

C-translit.h: C-translit.h.in gen-translit.pl
	$(PERL) gen-translit.pl < $< > $@.tmp
	mv -f $@.tmp $@

# The path to the compiled binary locale archive or compiled locales,
# along with the parent path to the source locales and source
# charmaps.
localepath = "$(complocaledir):$(i18ndir)"

# -Iprograms doesn't really belong here, but this gets it at the head
# of the list instead of the tail, where CPPFLAGS-$(lib) gets added.
# We need it before the standard -I's to see programs/config.h first.
locale-CPPFLAGS = -DCOMPLOCALEDIR='"$(complocaledir)"' \
		  -DLOCALE_ALIAS_PATH='"$(localedir)"' \
		  -Iprograms

CPPFLAGS-locale-programs = -DLOCALE_PATH='$(localepath)' \
			   -DCHARMAP_PATH='"$(i18ndir)/charmaps"' \
			   -DREPERTOIREMAP_PATH='"$(i18ndir)/repertoiremaps"' \
			   -DLOCSRCDIR='"$(i18ndir)/locales"'

CFLAGS-charmap.c += -Wno-write-strings -Wno-char-subscripts
CFLAGS-locfile.c += -Wno-write-strings -Wno-char-subscripts
CFLAGS-charmap-dir.c += -Wno-write-strings

# Set libof-* for each routine.
cpp-srcs-left := $(localedef-modules) $(localedef-aux) $(locale-modules) \
		 $(lib-modules)
lib := locale-programs
include $(patsubst %,$(..)libof-iterator.mk,$(cpp-srcs-left))