2009-10-16  John Dallaway  <john@dallaway.org.uk>

	* cdl/hal_arm_xscale_iq80310.cdl: Parent under
	CYGPKG_HAL_ARM_XSCALE_IOP310.

2003-09-23  Jani Monoses <jani@iv.ro>
	
        * src/diag/diag.c: Only use ethernet if CYGPKG_IO_ETH_DRIVERS
        is enabled.

2003-09-21  Gary Thomas  <gary@mlbassoc.com>

	* misc/redboot_RAM.ecm: 
	* misc/redboot_ROM.ecm:  Adjust for changes in RedBoot
	template - DNS now must be enabled manually.

2003-02-10  Nick Garnett  <nickg@calivar.com>

	* misc/redboot_ROMA.ecm:
	Changed reference to CYGSCYGSEM_HAL_ARM_IQ80310_ARMBOOT to
	CYGSEM_HAL_ARM_IOP310_ARMBOOT.

2003-02-05  Nick Garnett  <nickg@calivar.com>

	* src/diag/iq80310.h: Added CYGONCE_IQ80310_H to avoid compilation
	errors.

2003-01-31  Mark Salter  <msalter@redhat.com>

	* include/hal_platform_setup.h: Disabling of write buffer
	is not necessary.

	* misc/redboot_RAM.ecm: Don't enable BTB for RedBoot.
	* misc/redboot_RAMA.ecm: Ditto.
	* misc/redboot_ROM.ecm: Ditto.
	* misc/redboot_ROMA.ecm: Ditto.

2003-01-30  Mark Salter  <msalter@redhat.com>

	* include/pkgconf/mlt_*: Adjust RAM size to match max supported.
	Actual size of installed RAM determined at runtime.
	
2003-01-22  Mark Salter  <msalter@redhat.com>

	* src/diag/diag.c: Don't define DEFINE_VARS.
	* src/diag/pci_serv.c: Remove pci_int_handlers decl.
	* src/diag/iq80310.h: Remove cmd_stat declaration.
	* src/diag/flash.c: Declare cmd_stat.
	* include/plf_io.h: Remove unused duplicate code.
	(HAL_PCI_TRANSLATE_INTERRUPT): Fix typo.

2002-11-13  Mark Salter  <msalter@redhat.com>

	* misc/redboot_RAM.ecm: Remove CYGPKG_IO_SERIAL_ARM_XSCALE_IQ80310.
	* misc/redboot_RAMA.ecm: Ditto.
	* misc/redboot_ROM.ecm: Ditto
	* misc/redboot_ROMA.ecm: Ditto

	* cdl/hal_arm_xscale_iq80310.cdl (CYGBLD_INTEL_DIAGNOSTICS): Change
	default to 1.
	* include/hal_platform_setup.h: Use IOP310_EARLY_PCI_SETUP to make
	some BIOSes happy. BTB_INIT macro provided elsewhere.
	* src/diag/*: General cleanup to get rid of warnings and to eliminate
	functionality provided by the HAL. 

2002-11-12  Gary Thomas  <gary@mlbassoc.com>

	* src/diag/xscale_test.c: 
	* src/diag/test_menu.h: 
	* src/diag/test_menu.c: 
	* src/diag/pci_serv.c: 
	* src/diag/pci_bios.h: 
	* src/diag/memtest.c: 
	* src/diag/irq.S: 
	* src/diag/iq80310.h: 
	* src/diag/io_utils.c: 
	* src/diag/interrupts.c: 
	* src/diag/i557_eep.h: 
	* src/diag/i557_eep.c: 
	* src/diag/flash.c: 
	* src/diag/external_timer.c: 
	* src/diag/ether_test.h: 
	* src/diag/ether_test.c: 
	* src/diag/diag.c: 
	* src/diag/cycduart.h: 
	* src/diag/cycduart.c: 
	* src/diag/7_segment_displays.h: 
	* src/iq80310_misc.c: 
	* misc/redboot_ROMA.ecm: 
	* misc/redboot_ROM.ecm: 
	* misc/redboot_RAMA.ecm: 
	* misc/redboot_RAM.ecm: 
	* include/pkgconf/mlt_arm_xscale_iq80310_roma.mlt: 
	* include/pkgconf/mlt_arm_xscale_iq80310_roma.ldi: 
	* include/pkgconf/mlt_arm_xscale_iq80310_roma.h: 
	* include/pkgconf/mlt_arm_xscale_iq80310_rom.mlt: 
	* include/pkgconf/mlt_arm_xscale_iq80310_rom.ldi: 
	* include/pkgconf/mlt_arm_xscale_iq80310_rom.h: 
	* include/pkgconf/mlt_arm_xscale_iq80310_ram.mlt: 
	* include/pkgconf/mlt_arm_xscale_iq80310_ram.ldi: 
	* include/pkgconf/mlt_arm_xscale_iq80310_ram.h: 
	* include/plf_io.h: 
	* include/hal_platform_setup.h: 
	* include/hal_platform_ints.h: 
	* cdl/hal_arm_xscale_iq80310.cdl: Reorg under Xscale variants.

2002-09-19  Mark Salter  <msalter@redhat.com>

	* src/iq80310_misc.c (hal_hardware_init): Call hal_xscale_core_init.
	(iq80310_program_new_stack): Remove.
	Remove debug support which is now in xscale core package.
	* misc/redboot_RAM.ecm: Add CYGPKG_HAL_ARM_XSCALE_CORE package.
	* misc/redboot_RAMA.ecm: Ditto.
	* misc/redboot_ROM.ecm: Ditto.
	* misc/redboot_ROMA.ecm: Ditto.
	* include/plf_io.h (CYGARC_PHYSICAL_ADDRESS): Define.
	* include/hal_platform_setup.h (DCACHE_FLUSH_AREA): Remove define.
	Remove debug unit init code.
	* include/hal_iq80310.h (DCACHE_FLUSH_AREA): Define.
	* cdl/hal_arm_iq80310.cdl: Remove HAL_ARCH_PROGRAM_NEW_STACK and
	add CYGBLD_HAL_VAR_H.

2002-08-29  Mark Salter  <msalter@redhat.com>

	* include/plf_stub.h: Add HAL_STUB_HW_BREAKPOINT_LIST_SIZE and
	HAL_STUB_HW_WATCHPOINT_LIST_SIZE.

2002-08-12  Mark Salter  <msalter@redhat.com>

	* cdl/hal_arm_iq80310.cdl: Remove CYGSEM_REDBOOT_ARM_LINUX_BOOT ref.
	* misc/redboot_ROM.ecm: Ditto.
	* misc/redboot_RAM.ecm: Ditto.

2002-08-06  Gary Thomas  <gary@chez-thomas.org>
2002-08-06  Motoya Kurotsu <kurotsu@allied-telesis.co.jp>	

	* src/hal_diag.c: I/O channel data can't be constant - contains
	timeout information which can be changed.

2002-05-28  Mark Salter  <msalter@redhat.com>

	* cdl/hal_arm_iq80310.cdl: Add Linux boot support.
	* misc/redboot_RAM.ecm: Ditto.
	* misc/redboot_ROM.ecm: Ditto.

	* include/hal_iq80310.h (CYGARC_HAL_MMU_OFF): Xscale has
	special requirements for turning off MMU.

2002-05-24  Jonathan Larmour  <jlarmour@redhat.com>

	* src/hal_diag.c: Support dynamic getting and setting of baud rates.
	* cdl/hal_arm_iq80310.cdl: implements
	CYGINT_HAL_VIRTUAL_VECTOR_COMM_BAUD_SUPPORT

2002-05-14  Jesper Skov  <jskov@redhat.com>

	* include/plf_io.h (CYGARC_VIRT_TO_BUS, CYGARC_UNCACHED_ADDRESS):
	Fixed compiler warnings.

2002-05-07  Gary Thomas  <gthomas@redhat.com>

	* cdl/hal_arm_iq80310.cdl: 
	Standardize CYGNUM_HAL_VIRTUAL_VECTOR_CONSOLE_CHANNEL_DEFAULT usage.	

2002-04-22  Jonathan Larmour  <jlarmour@redhat.com>

	* misc/redboot_RAM.ecm: Enable GDB remote file I/O support.
	* misc/redboot_RAMA.ecm: Ditto.
	* misc/redboot_ROM.ecm: Ditto.
	* misc/redboot_ROMA.ecm: Ditto.

2002-04-16  John Dallaway  <jld@redhat.com>

	* cdl/hal_arm_iq80321.cdl: Use arm-elf toolchain by default.

2002-03-06  Jesper Skov  <jskov@redhat.com>

	* misc/redboot_RAM.ecm: Added dns and zlib support.
	* misc/redboot_ROM.ecm: Same.

2002-02-22  Mark Salter  <msalter@redhat.com>

	* src/iq80310_misc.c (cyg_hal_plf_hw_breakpoint): Fix use of wrong reg.

2002-02-06  Mark Salter  <msalter@redhat.com>

	* include/hal_platform_setup.h: Fix condition of some I2C bit tests.

2002-02-04  Mark Salter  <msalter@redhat.com>

	* include/hal_platform_setup.h: Fix bad insns in I2C code.

2002-01-28  Jesper Skov  <jskov@redhat.com>

	* src/iq80310_misc.c (hal_hardware_init): Fix warning.

	* cdl/hal_arm_iq80310.cdl: Removed explicit plf_io.h declaration.

2002-01-16  Hugo Tyson  <hmt@redhat.com>

	* include/hal_platform_ints.h (HAL_CLOCK_REINITIALIZE): Better
	names for macro args, and the freqency is now signed.  -ve means
	don't set the clock, just tell me what you would do.

	* src/iq80310_misc.c (hal_clock_reinitialize): Always return a
	nearby good value; don't set h/w if <0.  Convoluted logic changes
	to support that.

2002-01-14  Hugo Tyson  <hmt@redhat.com>

	* include/hal_platform_ints.h (HAL_CLOCK_REINITIALIZE): New macro
	which calls the below, also a prototype for it.

	* src/iq80310_misc.c (hal_clock_reinitialize): New routine to
	reset the clock to a different frequency.  This is for GPROF type
	profiling use only; not general purpose eCos usage.

2002-01-04  Mark Salter  <msalter@redhat.com>

	* include/hal_platform_setup.h: Turn on ECC for uncached alias of RAM.

2002-01-03  Mark Salter  <msalter@redhat.com>

	* misc/redboot_ROM.ecm: Use generic i82559 package.
	* misc/redboot_ROMA.ecm: Ditto.
	* misc/redboot_RAM.ecm: Ditto.
	* misc/redboot_RAMA.ecm: Ditto.

	* include/plf_io.h (CYGARC_UNCACHED_ADDRESS): New macro to return
	uncached alias for a cached address.
	(CYGARC_VIRT_TO_BUS): Macro to convert virtual to physical addresses.
	* include/hal_platform_setup.h: Add uncached alias for first 128M of
	SDRAM.

2001-10-03  Jonathan Larmour  <jlarmour@redhat.com>

	* src/diag/io_utils.c: Switch to diag_printf from printf.
	* src/diag/iq80310.h: Ditto.
	* src/diag/memtest.c: Ditto, and don't define printf prototype.

2001-08-27  Mark Salter  <msalter@redhat.com>

	* cdl/hal_arm_iq80310.cdl (CYGSEM_HAL_ARM_IQ80310_BTB): New option.
	(CYGSEM_HAL_ARM_IQ80310_CLEAR_PCI_RETRY) New option.
	
	* src/iq80310_pci.c (cyg_hal_plf_pci_init): Clear PCI retry based on
	CYGSEM_HAL_ARM_IQ80310_CLEAR_PCI_RETRY.

	* include/hal_platform_setup.h: Turn on BTB based on configure option.

2001-08-24  Mark Salter  <msalter@redhat.com>

	* src/iq80310_misc.c (iq80310_program_new_stack): Convert to inline
	asm so that code generation differences won't break it.

2001-08-15  Mark Salter  <msalter@redhat.com>

	* include/hal_iq80310.h: Fix size of PATUSR, SATUSR, PSR, and SSR regs.
	Make all register pointers volatile.

	* src/diag/flash.c: First page of flash now remapped to 0xd0000000.

2001-08-04  Mark Salter  <msalter@redhat.com>

	* include/hal_platform_setup.h: Fix mapping so first MB of SDRAM has
	ECC turned on. Now map first 4K of flash at 0xd0000000.

2001-06-21  Jonathan Larmour  <jlarmour@redhat.com>

	* images/*: Remove. Don't bloat repository with things already on
	the web.

2001-04-30  Gary Thomas  <gthomas@redhat.com>

	* include/hal_platform_setup.h: Remove #undef CYG_HAL_ROM_RESET_USES_JUMP
	since this is no longer used.

2001-04-18  Gary Thomas  <gthomas@redhat.com>

	* include/hal_platform_setup.h: Override CYG_HAL_ROM_RESET_USES_JUMP
	to avoid addressing problems with ROM startup mode.

2001-04-17  Mark Salter  <msalter@redhat.com>

	* cdl/hal_arm_iq80310.cdl: Implement CYGINT_HAL_ARM_MEM_REAL_REGION_TOP
	(CYGBLD_GLOBAL_CFLAGS): Add -ffunction-sections and -fdata-sections.
	* src/iq80310_misc.c (hal_arm_mem_real_region_top): New function.

2001-04-16  Gary Thomas  <gthomas@redhat.com>

	* cdl/hal_arm_iq80310.cdl: Add CDL to describe CPU family.

2001-04-10  Mark Salter  <msalter@redhat.com>

	* include/hal_platform_setup.h: Turn on multi-bit RAM error reporting.

2001-04-03  Mark Salter  <msalter@redhat.com>

	* src/diag/flash.c: Don't compile unless CYGPKG_IO_FLASH defined.
	* src/diag/xscale_test.c (testMenu): Only add flash_test if
	CYGPKG_IO_FLASH is defined.

2001-03-31  Mark Salter  <msalter@redhat.com>

	* src/diag/xscale_test.c: Merge in latest changes from Cyclone.
	* src/diag/iq80310.h: Ditto.
	* src/diag/external_timer.c: Ditto.

2001-03-30  Mark Salter  <msalter@redhat.com>

	* misc/redboot_RAM.ecm: Disable CYGSEM_REDBOOT_FIS_CRC_CHECK
	and CYGSEM_IO_FLASH_VERIFY_PROGRAM.
	* misc/redboot_RAMA.ecm: Ditto.
	* misc/redboot_ROM.ecm: Ditto.
	* misc/redboot_ROMA.ecm: Ditto.

	* include/pkgconf/mlt_arm_iq80310_rom.h: Fix heap1_SIZE.
	* include/pkgconf/mlt_arm_iq80310_ram.h Ditto: 
	* include/pkgconf/mlt_arm_iq80310_ram.mlt: Remove PCI window.

	* include/hal_platform_setup.h: Fix page table comment.

2001-03-12  Jonathan Larmour  <jlarmour@redhat.com>

	* src/iq80310_misc.c: Ensure case ranges have spaces around
	identifiers to allow correct parsing by compiler.

2001-02-27  Jonathan Larmour  <jlarmour@redhat.com>

	* src/diag/pci_bios.h: Remove CVS-unfriendly keyword substitutions

2001-02-23  Jesper Skov  <jskov@redhat.com>

	* include/hal_cache.h (HAL_FLASH_CACHES_OLD_MACROS):  This platform
	uses deprecated cache handling macros.

2001-02-23  Gary Thomas  <gthomas@redhat.com>

	* misc/redboot_ROMA.ecm: Renamed from redboot_ROMA.cfg

	* misc/redboot_RAMA.ecm: Renamed from redboot_RAMA.cfg

	* misc/redboot_ROM.ecm: Renamed from redboot_ROM.cfg

	* misc/redboot_RAM.ecm: Renamed from redboot_RAM.cfg

2001-02-13  Gary Thomas  <gthomas@redhat.com>

	* src/iq80310_misc.c (hal_IRQ_handler): 
	Return CYGNUM_HAL_INTERRUPT_NONE for spurious interrupts.

2001-02-08  Jesper Skov  <jskov@redhat.com>

	* src/hal_diag.c: Replace CYGSEM_HAL_DIAG_MANGLER_None with
	CYGDBG_HAL_DIAG_TO_DEBUG_CHAN.

2001-02-07  Mark Salter  <msalter@redhat.com>

	* src/diag/external_timer.c (counter_test): Fix printf format
	string to work with stripped down RedBoot printf.(counter_test):

2001-02-06  Mark Salter  <msalter@redhat.com>

	* src/diag/external_timer.c: Merged in Cyclone changes.
	* src/diag/interrupts.c: Ditto.
	* src/diag/memtest.c: Ditto.
	* src/diag/xscale_test.c: Ditto.

2001-02-02  Mark Salter  <msalter@redhat.com>

	* src/diag/xscale_test.c (seven_segment_display): Use volatile for
	delay loop variable to avoid optimizing it away.

	* src/diag/flash.c (flash_buffer): Change huge array (.bss) to a
	pointer to scratchpad RAM above RedBoot.

	* src/iq80310_misc.c (hal_hardware_init): Don't enable FIQ (for now).
	(cyg_hal_plf_is_stopped_by_hardware): Check for stopped by BKPT insn.

	* misc/redboot_ROM.cfg (CYGNUM_IO_ETH_DRIVERS_NUM_PKT): Set value to 2.
	* misc/redboot_ROMA.cfg: Ditto.
	* misc/redboot_RAM.cfg: Ditto.
	* misc/redboot_RAMA.cfg: Ditto.

2001-01-31  Mark Salter  <msalter@redhat.com>

	* src/iq80310_pci.c (__pci_abort_handler): Use naked attribute for
	use as abort handler.

	* src/iq80310_misc.c (_scrub_ecc): New function.
	(hal_IRQ_handler): Fix switched sensing of FIQ/IRQ.
	(hal_hardware_init): Install handlers for NMI FIQs. Fix	switched
	installation of FIQ/IRQ ISRs.

	* include/hal_iq80310.h (RFR_INIT_VAL): Double refresh interval.
	Add more register definitions.

	* include/hal_platform_setup.h: Add support for baterry test.
	Enable Yavapai single-bit error correction.

	* src/diag/*: Integrate latest Cyclone code. Add RHEPL to contributed
	files.

2001-01-31  Jesper Skov  <jskov@redhat.com>

	* src/hal_diag.c: Replaced CYGDBG_HAL_DIAG_DISABLE_GDB_PROTOCOL
	with CYGSEM_HAL_DIAG_MANGLER_None

	* include/hal_diag.h: Fix hal_delay_us declaration.

2001-01-26  Jesper Skov  <jskov@redhat.com>

	* src/hal_diag.c: Removed CYGSEM_HAL_VIRTUAL_VECTOR_DIAG check.
	* include/plf_stub.h: Moved reset macro to
	* include/hal_platform_ints.h: this file.

2001-01-11  Mark Salter  <msalter@redhat.com>

	* include/hal_platform_setup.h: Remove hardcoded position dependencies
	in page table setup.
	
	* cdl/hal_arm_iq80310.cdl (CYGSEM_HAL_ARM_IQ80310_ARMBOOT): New
	bool option. If true, modifies ROM startup so that we coexist with
	ARM bootloader.

	* include/pkgconf/mlt_arm_iq80310_roma.mlt: New file. ROM statrup
	with modified start address to coexist with ARM bootloader.
	* include/pkgconf/mlt_arm_iq80310_roma.h: Regenerated.
	* include/pkgconf/mlt_arm_iq80310_roma.ldi: Regenerated.

	* misc/redboot_ROMA.cfg: RedBoot configuration for ROM startup by
	ARM booloader in FLASH boot sector.
	* misc/redboot_RAMA.cfg: RedBoot configuration for RAM startup with
	ARM booloader in FLASH boot sector.

2001-01-08  Mark Salter  <msalter@redhat.com>

	* src/diag/diag.c (do_hdwr_diag): Turn off debug channel interrupt
	and reset PCI bus before calling Cyclone diag code.

	* src/diag/xscale_test.c (hdwr_diag): Uncomment call to
	sys_pci_device_init.

2001-01-05  Mark Salter  <msalter@redhat.com>

	* src/iq80310_misc.c (iq80310_program_new_stack): New function to
	setup stack for programs called by RedBoot.
	* cdl/hal_arm_iq80310.cdl: Add define for HAL_ARCH_PROGRAM_NEW_STACK.
	(Merged from XScale branch).
	
	* cdl/hal_arm_iq80310.cdl: Add compile of Cyclone diag code.
	* src/diag: New directory with IQ80310 hw diag code from Cyclone.

2000-12-21  Mark Salter  <msalter@redhat.com>

	* src/iq80310_pci.c (cyg_hal_plf_pci_init): Play nice with PC BIOS.
	(pci_config_cleanup): Don't use fixed bus numbers.

	* include/plf_io.h (HAL_PCI_TRANSLATE_INTERRUPT): Don't use fixed
	secondary bus number.

	* include/hal_platform_setup.h: Increase reset delay to 60ms.
	Remove dead code.

2000-11-22  Mark Salter  <msalter@redhat.com>

	* src/hal_diag.c: Support 57600 baud.
	* cdl/hal_arm_iq80310.cdl: Accept 57600 as legal baudrate.

	* misc/redboot_RAM.cfg: Set CYGBLD_REDBOOT_MIN_IMAGE_SIZE to 0x40000.
	* misc/redboot_ROM.cfg: Ditto.

2000-11-19  Mark Salter  <msalter@redhat.com>

	* src/iq80310_misc.c (hal_clock_read): Fix timer bit juggling.

2000-11-19  Gary Thomas  <gthomas@redhat.com>

	* cdl/hal_arm_iq80310.cdl: Define CYGBLD_HAL_PLATFORM_IO_H.

2000-11-16  Mark Salter  <msalter@redhat.com>

	* src/iq80310_misc.c: Add support for external timer as RTC.
	(nirq_ISR): Correct dispatch for X3 interrupts.

	* include/hal_platform_ints.h (CYGNUM_HAL_INTERRUPT_RTC): Use ext timer.
	(HAL_DELAY_US): Define.

	* cdl/hal_arm_iq80310.cdl: Correct CYGNUM_HAL_RTC_PERIOD.

2000-11-06  Mark Salter  <msalter@redhat.com>

	* misc/redboot_RAM.cfg: Turn on CYGSEM_REDBOOT_BSP_SYSCALLS.
	* misc/redboot_ROM.cfg: Ditto.

2000-11-04  Mark Salter  <msalter@redhat.com>

	* misc/redboot_RAM.cfg: Add in PCI and ethernet.
	* misc/redboot_ROM.cfg: Ditto.

	* include/plf_io.h: Fleshed out PCI support.

	* cdl/hal_arm_iq80310.cdl: Add iq80310_pci.C for compile.
	Change default baud to 115200.

	* src/iq80310_pci.c: New file. HAL pci support.

	* include/plf_stub.h: Reworked HW watchpoint/breakpoint support.

	* src/iq80310_misc.c (hal_hardware_init): Remove DSU setup.
	(cyg_hal_plf_hw_watchpoint): Support one range instead of two
	single byte locations.
	(cyg_hal_plf_is_stopped_by_hardware): Rework interface to return
	reason for hardware stop and data address.

	* include/hal_platform_setup.h (PLATFORM_SETUP1): Clear DSU state.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2009 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================