2010-03-25  Daniel Helgason  <dhelgason@shaw.ca>

	* src/devs_flash_atmel_dataflash.c: Correct bad sector count for
	AT45DB642 dataflash device.
	* cdl/devs_flash_atmel_dataflash.cdl: Mark CYGPKG_IO_FLASH as the
	parent of this package.

2005-06-29  Jani Monoses <ani@iv.ro>

	* include/dataflash.h: Allow the package to be compiled without
	io/flash. Return correct value from cyg_dataflash_get_page_count()

2004-12-02  Bart Veer  <bartv@ecoscentric.com>

	* include/dataflash.h,
	src/devs_flash_atmel_dataflash_flash_dev_funs.c: include
	<cyg/io/flash_dev.h> explicitly rather than using _FLASH_PRIVATE_

2004-11-29  Bart Veer  <bartv@ecoscentric.com>

	(df_flash_hwr_map_error): this is now internal to the driver, no
	longer needed by the generic flash code.
	* src/devs_flash_atmel_dataflash_flash_dev_funs.c: use the dummy
	query/lock/unlock functions provided by the generic flash code

2004-11-22  Bart Veer  <bartv@ecoscentric.com>

	* include/dataflash.h, src/devs_flash_atmel_dataflash.c,
	src/devs_flash_atmel_dataflash_flash_dev_funs.c: merge the config
	and priv structures, removing the duplicate spi_dev data in the
	process. Adjust device driver API as per changes to the generic
	flash code.
	* src/devs_flash_atmel_dataflash_flash_dev_funs.c (df_flash_init):
	Rename cyg_block_info to cyg_flash_block_info

2004-11-21  Bart Veer  <bartv@ecoscentric.com>

	* cdl/devs_flash_atmel_dataflash.cdl: CYGHWR_IO_FLASH_DEVICE_V2 is
	now implicit

2004-11-20  Bart Veer  <bartv@ecoscentric.com>

	* cdl/devs_flash_atmel_dataflash.cdl: data flash requires indirect
	read support in the main flash code.

2004-10-07  Savin Zlobec  <savin@elatec.si> 

        * include/dataflash.h:
        * src/devs_flash_atmel_dataflash.c:
        Changed the API to be more consistent, included error
        reporting and added blocking/non blocking mode of operation.
        * src/devs_flash_atmel_dataflash_flash_dev_funs.c:
        Synced with new API and set the block size to DataFlash's
        native page size.

2004-10-07  Andrew Lunn  <andrew.lunn@ascom.ch>

	* cdl/devs_flash_atmel_dataflash.cdl: Remove
	CYGSEM_IO_FLASH_READ_INDIRECT which only legacy drivers should use
	when they provide a flash_read_buf function. For V2 drivers
	providing a read function in the device structure is sufficient.

2004-09-07  Savin Zlobec  <savin@elatec.si> 

        * cdl/devs_flash_atmel_dataflash.cdl:
        * include/dataflash.h:
        * src/devs_flash_atmel_dataflash.c:  
        * src/devs_flash_atmel_dataflash_flash_dev_funs.c:
        Atmel DataFlash driver implementation.   	 


//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================