2009-04-02  John Dallaway  <john@dallaway.org.uk>

	* cdl/spi_at91.cdl: Fix typographical error for
	CYGINT_DEVS_SPI_ARM_AT91_HAS_BUS1. [ Bugzilla 1000737 ]

2009-02-16  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/spi_at91.c (cyg_spi_at91_bus_init): Partially revert change of
	2009-02-11. Define an empty CYGBLD_ATTRIB_C_INIT_PRI and rely on
	spi_at91_init.cxx to call, in case the compiler does not supply
	that macro (e.g. if too old).
	* cdl/spi_at91.cdl: Revert change of 2009-02-11.
	* src/spi_at91_init.cxx: Revive. Set priority to CYG_INIT_BUS_SPI.
	Conditionalise on CYGBLD_ATTRIB_C_INIT_PRI.

2009-02-12  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/spi_at91.cdl: Add a requires for CYGPKG_ERROR.

2009-02-11  Bart Veer  <bartv@ecoscentric.com>

	* src/spi_at91.c (cyg_spi_at91_bus_init): turn into a prioritized
	constructor, make it a static and rename.

	* cdl/spi_at91.cdl: remove src/spi_at91_init.cxx
	
	* src/spi_at91_init.cxx: removed, no longer needed.

2008-10-19  Igor B. Poretsky <poretsky@mlbox.ru>
	
	* src/spi_at91.c: Typo fixes from var_io.h.  Correctly calculate
	  the board rate. Before it was two times too fast.

2006-09-27  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/spi_at91.c (spi_at91_transaction_begin): Don't use #ifdef
	inside a macro invocation. The compiler throws a wobbly.

2006-09-07  John Eigelaar <jeigelaar@mweb.co.za>

	* src/spi_at91.c: Fixed the chip select functions.
	Changed the Mode Register setup as to disable the Mode Failure
	Detaction for variants that support it. The Mode Failure Detection
	breaks because NPCS0 is not connected, we are using GPIO, and is 
	thus floating. 

2006-06-01  John Eigelaar <jeigelaar@mweb.co.za>

	* src/spi_at91.c:
	* cdl/spi_at91.cdl:
	* include/spi_at91.h: Generalize so that multiple SPI
	busses can be driven.
	
2006-05-19  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/spi_at91.c: Use the AT91 GPIO/PIO macros to aid
	portability between different AT91 device.

2004-11-11  Sebastian Block <sebastianblock@gmx.net>

        * src/spi_at91.c: Fixed negation of the chip select signal when
	not using a 4 to 16 decoder

2004-10-13  Savin Zlobec  <savin@elatec.si> 

        * src/spi_at91.c: Fixed a typo in spi_at91_transfer reported by
        Nicolas Brouard.

2004-08-31  Savin Zlobec  <savin@elatec.si> 

        * include/spi_at91.h:
        * src/spi_at91.c:
        Moved SPI registers and bits defines to HAL headers, added support 
        for 4 to 16 decoder of chip select signals, support for transfers 
        larger than 2^16 and per device configurable delay between two 
        transfers.  
        * cdl/spi_at91.cdl: 
        Added option to enable support for 4 to 16 decoder of chip select 
        signals.  

2004-08-27  Savin Zlobec  <savin@elatec.si> 

        * cdl/spi_at91.cdl:
        * include/spi_at91.h:
        * src/spi_at91.c:
        * src/spi_at91_init.cxx:
        Atmel AT91 SPI bus driver implementation.   	 



//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2009 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================