2010-05-10  Ross Younger  <wry@ecoscentric.com>

	* include/string.h: Declare strnlen.
	* include/stringsupp.hxx: Declare __strnlen.
	* src/strnlen.cxx, tests/strnlen.c: Created.
	* cdl/string.cdl (CYGFUN_LIBC_STRING_GNU_STRNLEN): New option,
	compiles strnlen.cxx.
	(CYGPKG_LIBC_STRING_TESTS): Add strnlen test.

2009-01-26  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/memchr.c (main): Rename to cyg_user_start if main isn't
	going to be called.
	* tests/memcmp1.c (main): Ditto.
	* tests/memcmp2.c (main): Ditto.
	* tests/memcpy1.c (main): Ditto.
	* tests/memcpy2.c (main): Ditto.
	* tests/memmove1.c (main): Ditto.
	* tests/memmove2.c (main): Ditto.
	* tests/memset.c (main): Ditto.
        * tests/strcat1.c (main): Ditto.
        * tests/strcat2.c (main): Ditto.
        * tests/strchr.c (main): Ditto.
        * tests/strcmp1.c (main): Ditto.
        * tests/strcmp2.c (main): Ditto.
        * tests/strcoll1.c (main): Ditto.
        * tests/strcoll2.c (main): Ditto.
        * tests/strcpy1.c (main): Ditto.
        * tests/strcpy2.c (main): Ditto.
        * tests/strcspn.c (main): Ditto.
        * tests/strlen.c (main): Ditto.
        * tests/strncat1.c (main): Ditto.
        * tests/strncat2.c (main): Ditto.
        * tests/strncpy1.c (main): Ditto.
        * tests/strncpy2.c (main): Ditto.
        * tests/strpbrk.c (main): Ditto.
        * tests/strrchr.c (main): Ditto.
        * tests/strspn.c (main): Ditto.
        * tests/strstr.c (main): Ditto.
        * tests/strtok.c (main): Ditto.
        * tests/strxfrm1.c (main): Ditto.
        * tests/strxfrm2.c (main): Ditto.

2005-07-22  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/strcmp.cxx (__strcmp): Set retval to zero to avoid compiler
	warnings.

2004-02-20  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/string.h: Prototype strdup().
	* include/stringsupp.hxx: Prototype __strdup().
	externC -> __externC while I'm here.
	* src/strdup.cxx: New file implementing strdup()/__strdup().
	* cdl/string.cdl: Build strdup.cxx if CYGINT_ISO_MALLOC.

	* src/strtok.cxx (strtok): Use correct thread data type.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/string.cdl: Fix doc link.

2001-11-27  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/string.cdl (CYGFUN_LIBC_STRING_BSD_FUNCS): New option to indicate
	provision of BSD-ish string functions.
	* include/bsdstring.h: New header to export BSD string func prototypes.
	* src/bsdstring.cxx: New file.

2001-08-21  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/string.cdl (CYGSEM_LIBC_STRING_PER_THREAD_STRTOK): Improve
	dependencies.

2001-08-10  Robin Farine  <acnrf@dial.eunet.ch>

	* src/memchr.cxx (__memchr): Don't check string validity if number
	of bytes to operate on is 0.
	* src/memcmp.cxx (__memcmp): Ditto.
	* src/memmove.cxx (__memmove): Ditto.
	* src/strncat.cxx (__strncat): Ditto.
	* src/strncmp.cxx (__strncmp): Ditto.
	* src/strncpy.cxx (__strncpy): Ditto.
	* src/strxfrm.cxx (__strxfrm): Ditto.

2000-05-20  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* src/strtok.cxx: Remove aliases

2000-05-02  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* New package
	Separated original libc out into separate packages on functional
	boundaries.
	Header files are now managed by isoinfra package
	Plenty of cleanups done, but no major functionality changes

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================