2011-03-08  John Dallaway  <john@dallaway.org.uk>

	* cdl/lwip_net.cdl: Require CYGPKG_ISOINFRA.
	* include/arch/cc.h: Define ERRNO if CYGINT_ISO_ERRNO is
	implemented. Based on patch from Will Wagner. [ Bugzilla 1001169 ]

2011-01-30  Ilija Kocho  <ilijak@siva.com.mk>

	* cdl/lwip_net.cdl: New CDL option CYGSEM_LWIP_MEM_SECTION.
	* include/lwipopts.h: Enter MEM_SECTION entity.
	* src/mem.c, src/memp.c: Add an ability to use GCC section
	attribute for statically allocated buffers, pbufs, and heap.

2011-01-02  Ilija Kocho  <ilijak@siva.com.mk>

	* src/ecos/sequential.c, src/ecos/simple.c: Fixed miltiple-line
	comment warnings.

2010-12-10  Christophe Coutand  <ccoutand@stmi.com>

	* include/lwipopts.h: Fix compilation error when compiling SNMP
	code.

2010-08-02  John Dallaway  <john@dallaway.org.uk>

	* include/network.h: Match braces when including from C++ code.
	Issue reported by Will Wagner.

2010-02-07  John Dallaway  <john@dallaway.org.uk>

	* cdl/lwip_net.cdl: Rename CFLAGS_ADD and CFLAGS_REMOVE options to
	match package macro name.

2010-01-25  Simon Kallweit  <simon.kallweit@intefo.ch>

	* all: Updated to lwIP 1.3.2

2007-03-22  John Eigelaar  <jeigelaar@mweb.co.za>
                                                     
	* include/lwip/netif.h, include/lwip/inet.h: Added externC macro
	to public fucntions to make them C++ compliant.

2006-05-09  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/ecos/init.c (arp_timer): Only compile this function when
	Ethernet is supported.
	* include/lwipopts.h: PAP_SUPPORT & CHAP_SUPPORT must be either 0
	or 1 otherwise we get compiler errors.
	
2006-03-26  Uwe Kindler <uwe_kindler@web.de>

	* Updated the complete lwIP source to the latest lwIP
	CVS version 1.1.1
	* src/ecos/init.c Added call to netif_set_up(netif) in
	function lwip_set_addr() - this is required since lwIP
	version 1.0.0
	* cdl/lwip_net.cdl Minor modifications for UDP configuration
	options. Renamed CYGNUM_LWIP_TCPIP_THREAD_PRIORITY to
	CYGNUM_LWIP_NETWORK_THREAD_PRIORITY and moved option outside
	CYGPKG_LWIP_TCPIP component because the network thread needs to
	run in all configurations.
	* tests/nc_slave.c
	* tests/tcpecho.c 
	* tests/udpecho.c
	* tests/sockets.c
	* tests/httpd.c Added eCos test infrastructure to tests and 
	made tests applicable depending on lwip configuration.

2006-03-15  Andrew Lunn  <andrew.lunn@ascom.ch>

	* tests/nc_test_slave.c (nc_slave): Fix some of the compiler
	warnings.

2006-03-13  Uwe Kindler <uwe_kindler@web.de>

	* cdl/lwip_net.cdl Changed default value of 
	CYGNUM_LWIP_MEMP_NUM_SYS_TIMEOUT (required for DHCP). 
	Replaced CYGPKG_LWIP_DHCP_OPTIONS with CYGPKG_LWIP_DHCP 
	and add CYGOPT_LWIP_DHCP_MANAGEMENT for automatic DHCP
	management.
	* include/lwip/ip_addr.h Add macro ip_addr_netcmp() 
	(copied from lwIP CVS).
	* include/netif/etharp.h Updated file to version of
	lwIP CVS.
	* src/ecos/init.c Add include <pkgconf/net_lwip.h>
	Add lwip_dhcp_fine_tmr() and lwip_dhcp_coarse_tmr()
	for DHCP processing.
	Change tcpip_init_done() to start DHCP timers and
	ARP timer.
	Changed lwip_set_addr() to properly setup IP adress
	if DHCP is used.
	Added lwip_dhcp_init() for start of DHCP client.
	Removed start of ARP timer from ecosclue_init().
	* src/netif/etharp.c Updated file to version of
	lwIP CVS.
	
2006-03-02  Andrew Lunn  <andrew.lunn@ascom.ch>

	* cdl/lwip_net.cdl: Add the interfaces CYGPKG_NET_STACK,
	CYGPKG_NET_STACK_INET and CYGPKG_NET_STACK_INET6 and say that we
	implement a network stack and an IPv4 stack. Without these interfaces
	some of the Ethernet device drivers won't be compiled.

2006-02-24  Uwe Kindler <uwe_kindler@web.de>

	* cdl/lwip_net.cdl: Changed names of configuration options
	according to eCos configuration option naming convention in 
	component writers guide.
	* include/lwipopts.h: Changed mapping of eCos configuration
	parameters to lwip configuration parameters. The mapping
	was wrong because it expected a disabled eCos configuration
	option is defined as 0 but a disabled eCos configuration option
	is not defined.
	* include/lwip/api.h Enumeration values of netconn_type are
	defined conditional now to avoid compiler warnings if these
	values are not evaluated in a switch statement.
	* src/api/api_lib.c Compilation of code in several switch 
	statements is now conditional depending on configured 
	functionality.
	* src/api/sockets.c Compilation of some code is now conditional 
	depending on configured functionality.
	* src/ecos/init.c Changed initialisation values to match the
	new configuration option names.

2005-10-07  Uwe Kindler <uwe_kindler@web.de>

	* src/core/tcp_in.c: pbuf_free() assert triggered by 
	NULLified inseg.p
	* include/lwip/tcp.h Do no longer try to free pbuf 
	when TCP_EVENT_RECV() is called without a callback 
	handler, and without packet. 
	* tests/nc_test_slave.c Fixed test_printf and diag_printf
	format strings that caused errors or warnings.
	* tests/nc_test_slave.c Included <lwip/inet.h> - required
	for compilation
	* src/ecos/init.c Added structs ip_addr ipaddr, netmask and gw
	in lwip_init() if loop interface is used

2004-05-05  Jani Monoses <jani@iv.ro>

	* src/netif/ppp/ppp.c: Decrease sleep period in main thread
	from 250ms to 1ms. Was a leftover of debugging the code and
	slowing things down.

2004-05-04  Jani Monoses <jani@iv.ro>

	* cdl/lwip_net.cdl
	* src/api/err.c
	* src/api/tcpip.c
	* src/api/sockets.c
	* src/api/api_lib.c
	* src/api/api_msg.c
	* src/core/tcp_in.c
	* src/core/ipv4/ip.c
	* src/core/ipv4/ip_addr.c
	* src/core/ipv4/ip_frag.c
	* src/core/ipv4/icmp.c
	* src/core/tcp_out.c
	* src/core/mem.c
	* src/core/raw.c
	* src/core/tcp.c
	* src/core/sys.c
	* src/core/udp.c
	* src/core/stats.c
	* src/core/dhcp.c
	* src/core/netif.c
	* src/core/inet.c
	* src/core/memp.c
	* src/core/pbuf.c
	* src/ecos/sio.c
	* src/ecos/sys_arch.c
	* src/ecos/init.c
	* src/netif/ppp/vj.c
	* src/netif/ppp/vj.h
	* src/netif/ppp/randm.c
	* src/netif/ppp/randm.h
	* src/netif/ppp/vjbsdhdr.h
	* src/netif/ppp/fsm.c
	* src/netif/ppp/fsm.h
	* src/netif/ppp/lcp.c
	* src/netif/ppp/lcp.h
	* src/netif/ppp/md5.c
	* src/netif/ppp/md5.h
	* src/netif/ppp/pap.c
	* src/netif/ppp/pap.h
	* src/netif/ppp/ppp.c
	* src/netif/ppp/ppp.h
	* src/netif/ppp/magic.c
	* src/netif/ppp/magic.h
	* src/netif/ppp/pppdebug.h
	* src/netif/ppp/auth.c
	* src/netif/ppp/auth.h
	* src/netif/ppp/chap.c
	* src/netif/ppp/chap.h
	* src/netif/ppp/ipcp.c
	* src/netif/ppp/ipcp.h
	* src/netif/ppp/chpms.c
	* src/netif/ppp/chpms.h
	* src/netif/etharp.c
	* src/netif/slipif.c
	* src/netif/loopif.c
	* tests/tcpecho.c
	* tests/udpecho.c
	* tests/nc_test_framework.h
	* tests/nc_test_slave.c
	* tests/httpd.c
	* tests/sys_timeout.c
	* tests/socket.c
	* include/arch/cc.h
	* include/arch/sys_arch.h
	* include/arch/perf.h
	* include/lwip/ip.h
	* include/lwip/debug.h
	* include/lwip/ip_addr.h
	* include/lwip/api.h
	* include/lwip/def.h
	* include/lwip/err.h
	* include/lwip/mem.h
	* include/lwip/opt.h
	* include/lwip/ip_frag.h
	* include/lwip/raw.h
	* include/lwip/sio.h
	* include/lwip/tcp.h
	* include/lwip/sys.h
	* include/lwip/udp.h
	* include/lwip/tcpip.h
	* include/lwip/stats.h
	* include/lwip/arch.h
	* include/lwip/dhcp.h
	* include/lwip/netif.h
	* include/lwip/icmp.h
	* include/lwip/inet.h
	* include/lwip/memp.h
	* include/lwip/pbuf.h
	* include/lwip/snmp.h
	* include/lwip/sockets.h
	* include/lwip/api_msg.h
	* include/netif/etharp.h
	* include/netif/slipif.h
	* include/netif/loopif.h
	* include/network.h
	* include/lwipopts.h : Initial import of the lwIP TCP/IP stack.

//===========================================================================
//####ECOSGPLCOPYRIGHTBEGIN####
// -------------------------------------------
// This file is part of eCos, the Embedded Configurable Operating System.
// Copyright (C) 2004, 2010, 2011 Free Software Foundation 
//
// eCos is free software; you can redistribute it and/or modify it under
// the terms of the GNU General Public License as published by the Free
// Software Foundation; either version 2 or (at your option) any later version.
//
// eCos is distributed in the hope that it will be useful, but WITHOUT ANY
// WARRANTY; without even the implied warranty of MERCHANTABILITY or
// FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public License
// for more details.
//
// You should have received a copy of the GNU General Public License along
// with eCos; if not, write to the Free Software Foundation, Inc.,
// 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA.
//
// As a special exception, if other files instantiate templates or use macros
// or inline functions from this file, or you compile this file and link it
// with other works to produce a work based on this file, this file does not
// by itself cause the resulting work to be covered by the GNU General Public
// License. However the source code for this file must still be made available
// in accordance with section (3) of the GNU General Public License.
//
// This exception does not invalidate any other reasons why a work based on
// this file might be covered by the GNU General Public License.
//
// -------------------------------------------
//####ECOSGPLCOPYRIGHTEND####
//===========================================================================