2009-10-16  John Dallaway  <john@dallaway.org.uk>

	* cdl/hal_arm_xscale_uE250.cdl: Parent under
	CYGPKG_HAL_ARM_XSCALE_PXA2X0.

2009-01-31  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_arm_xscale_uE250.cdl: update compiler flags for gcc 4.x

2009-01-24  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_arm_xscale_uE250.cdl: switch from arm-elf-gcc to
	arm-eabi-gcc.

2009-01-24  Bart Veer  <bartv@ecoscentric.com>

	* src/vga_support.c: fix build problem with latest toolchains.

2003-09-21  Gary Thomas  <gary@mlbassoc.com>

	* misc/redboot_RAM.ecm: 
	* misc/redboot_ROM.ecm:  Adjust for changes in RedBoot
	template - DNS now must be enabled manually.

2003-09-20  Gary Thomas  <gary@mlbassoc.com>

	* src/uE250_ide.c: IDE init needs to return number of controllers found.

2003-08-08  Gary Thomas  <gary@mind.be>

	* src/uE250_pci.c: 
	* src/uE250_misc.c: Improve PCI initialization, including support
	for external bus masters.

	* include/plf_io.h: Define CYGARC_PCI_DMA_ADDRESS()

2003-05-28  Gary Thomas  <gary@mind.be>

	* src/xilinx-load.c: Improve feedback during FPGA downloads.

2003-03-08  Gary Thomas  <gary@mind.be>

	* include/pkgconf/mlt_arm_xscale_uE250_ram.mlt: 
	* include/pkgconf/mlt_arm_xscale_uE250_ram.ldi: 
	* include/pkgconf/mlt_arm_xscale_uE250_ram.h: RAM limits were wrong.

2003-02-28  Gary Thomas  <gary@mind.be>

	* cdl/hal_arm_xscale_uE250.cdl: Fix machine type - used by Linux.	

2003-02-26  Gary Thomas  <gary@mind.be>

	* misc/redboot_ROM.ecm: 
	* misc/redboot_RAM.ecm: Update - larger RedBoot image now required.

2003-02-25  Gary Thomas  <gary@mind.be>

	* src/vga_support.c (vga_on): Fix screen enable/disable code.

	* src/uE250_pci.c: Initialize super I/O chip - used for legacy devices.

	* src/font.h: 
	* src/banner.xpm: 
	* src/vga_support.c: 
	* include/vga_support.h: New file(s) for VGA console support.

	* src/uE250_plx.c: 
	* cdl/hal_arm_xscale_uE250.cdl: Add support for console using VGA+PS/2.

2003-02-24  Gary Thomas  <gary@mind.be>

	* include/plx.h: Clean up unused code.

	* src/uE250_pci.c: 
	* src/uE250_misc.c: 
	* include/plf_io.h: 
	* include/hal_plf_ints.h: Support interrupts via PCI bus.

2003-02-04  Gary Thomas  <gary@mind.be>

	* src/xilinx-load.c: 
	* src/uE250_plx.c: 
	* src/uE250_pci.c: 
	* src/uE250_misc.c: 
	* src/uE250_ide.c: 
	* src/uE250_plx_bitstream.h: 
	* src/uE250_pci_bitstream.h: 
	* misc/redboot_ROM.ecm: 
	* misc/redboot_RAM.ecm: 
	* include/pkgconf/mlt_arm_xscale_uE250_romram.mlt: 
	* include/pkgconf/mlt_arm_xscale_uE250_romram.ldi: 
	* include/pkgconf/mlt_arm_xscale_uE250_romram.h: 
	* include/pkgconf/mlt_arm_xscale_uE250_rom.mlt: 
	* include/pkgconf/mlt_arm_xscale_uE250_rom.ldi: 
	* include/pkgconf/mlt_arm_xscale_uE250_rom.h: 
	* include/pkgconf/mlt_arm_xscale_uE250_ram.mlt: 
	* include/pkgconf/mlt_arm_xscale_uE250_ram.ldi: 
	* include/pkgconf/mlt_arm_xscale_uE250_ram.h: 
	* include/uE250.h: 
	* include/plx.h: 
	* include/plf_mmap.h: 
	* include/hal_plf_ints.h: 
	* include/plf_io.h: 
	* include/hal_platform_setup.h: 
	* cdl/hal_arm_xscale_uE250.cdl: 
	New package - support for NMI uE250 (Xscale PXA250) platform.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2009 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================