Disk Channel Structure

Each physical disk connected to a controller is represented by a disk channel. Each channel is defined with the following macro:

DISK_CHANNEL(l, funs, dev_priv, controller, mbr_supp, max_part_num )

Arguments

l

The "C" label for this structure.

funs

The set of interface functions (see below).

dev_priv

A placeholder for any device specific data for this channel.

controller

Pointer to controller to which this disk channel is attached.

mbr_supp

Does this disk support partitioning.

max_part_num

The maximum number of partitions to be supported.

The interface from the hardware independent driver into the hardware interface module is contained in the funs table. This is defined by the DISK_FUNS macro.

If the space for the channel has been allocated elsewhere, the following macro may be used to initialise it:
DISK_CHANNEL_INIT(dc, funs, dev_priv, controller, disk_info, part_dev_tab, part_chan_tab, part_tab, mbr_supp, max_part_num )

The arguments are as for DISK_CHANNEL() except for the following:

Arguments

dc

The name of an object of type disk_channel. This object will be initialised by the macro.

disk_info

The name of an object of type disk_info.

part_dev_tab

The name of an array of objects of type struct cyg_devtab_entry. The number of array members must equal max_part_num, plus one.

part_chan_tab

The name of an array of objects of type disk_channel. The number of array members must equal max_part_num.

part_tab

The name of an array of objects of type cyg_disk_partition_t. The number of array members must equal max_part_num.