DISK_FUNS(l, read, write, get_config, set_config) |
Arguments
lThe "C" label for this structure.
readCyg_ErrNo (*read)(disk_channel *priv, void *buf, cyg_uint32 len, cyg_uint32 block_num)
This function reads len sectors of data from the disk at the sector number given by block_num. The actual quantity of data transferred depends on the disk's sector size, which can be obtained using the CYG_IO_GET_CONFIG_DISK_INFO key.
If the read completes immediately, or the low level driver is configured to do all IO synchronously, this function will return ENOERR, and if it fails will return a negative error code, for example -EIO. If the function returns -EWOULDBLOCK then it has only started the transfer and will indicate its completion by calling the transfer_done callback.
writeCyg_ErrNo (*write)(disk_channel *priv, void *buf, cyg_uint32 len, cyg_uint32 block_num)
This function writes len sectors of data to the disk at the block given by block_num. The actual quantity of data transferred depends on the disk's sector size, which can be obtained using the CYG_IO_GET_CONFIG_DISK_INFO key.
If the write completes immediately, or the low level driver is configured to do all IO synchronously, this function will return ENOERR, and if it fails will return a negative error code, for example -EIO. If the function returns -EWOULDBLOCK then it has only started the transfer and will indicate its completion by calling the transfer_done callback.
get_configbool (*get_config)(serial_channel *priv, cyg_uint32 key, const void *xbuf, cyg_uint32 *len); )
This function is used to get configuration data from the device. The key argument defines the configuration data to be fetched. The xbuf and *len arguments describe a buffer into which the data will be put. The function should return true if the key type is supported and the buffer of sufficient length to contain the data. The value of *len should be updated to actual length of the data returned. The function should return false if the driver cannot support the key value or the buffer is of insufficient length.
The following keys may be used to get information from a disk device.
This key causes a cyg_disk_info_t
structure, as defined in diskio.h to
be returned.
This key returns a copy of the
cyg_disk_event_t previously set
by CYG_IO_SET_CONFIG_DISK_EVENT.
set_configbool (*set_config)(serial_channel *priv, cyg_uint32 key, const void *xbuf, cyg_uint32 *len); )
This function is used to change the configuration of the device. The key argument defines the kind of configuration data to be set. The xbuf and *len arguments describe a buffer in which the data is supplied. The function should return true if the key type is supported and the buffer of the correct length and the data appears valid. The function should return false if the driver cannot support the key value or the buffer is the wrong length, or the data is invalid in some other way.
The following keys can be sent to a driver:
This is invoked from the filesystem after locating the device driver to record that the device has been mounted. The generic device layer records the mount against both the partition and physical disk and passes the call on down to the driver. The xbuf and *len arguments are unused.
This is invoked from the filesystem to record that the
device has been unmounted. The generic device layer
records the unmount against both the partition and
physical disk and passes the call on down to the
driver. If the chan->info->mounts
counter is zero, the driver should call the
disk_disconnected() callback to
prepare the generic layer for a potential media
change. The xbuf and
*len arguments are unused.
This may be invoked by the application to set a disk event
callback function. The generic disk layer is mostly
responsible for handling this by recording the event
function in the disk channel structure. The call is
additionally passed down to the hardware driver so that it
may prepare the hardware, if necessary. The
xbuf should point to a
cyg_disk_event_t structure.