| eCosPro® Reference Manual | ||
|---|---|---|
| Prev | ||
#include <cyg/flashsafe/flashsafe.h>
|
int cyg_flashsafe_init(cyg_flashsafe *flashsafe);
int cyg_flashsafe_data(cyg_flashsafe *flashsafe, cyg_flashsafe_key key, void **data);
int cyg_flashsafe_read(cyg_flashsafe *flashsafe, cyg_flashsafe_key key, void *data, cyg_uint32 *len);
int cyg_flashsafe_open(cyg_flashsafe *flashsafe);
int cyg_flashsafe_write(cyg_flashsafe *flashsafe, cyg_flashsafe_key key, void *data, cyg_uint32 len);
int cyg_flashsafe_commit(cyg_flashsafe *flashsafe);
const char *cyg_flashsafe_errmsg(int err);
The flash safe is accessed through this API. The flashsafe is
initialized by calling cyg_flashsafe_init()
passing it a pointer to a cyg_flashsafe
structure. Within this structure the
base,
block_count and
block_size fields must have been
initialized to describe the area of flash to be
managed. Typically, the structure would be defined statically as
follows:
cyg_flashsafe flashsafe =
{
.base = 0x40000000,
.block_count = 3,
.block_size = 0x2000
};
|
If the flashsafe already contains data, then items may be
retrieved using cyg_flashsafe_data(). The
key argument identifies the data item to be
retrieved. The data argument is a pointer
to a location where a pointer to the data will be
stored. Typically the pointer returned will refer directly to the
flash device, and will thus be read-only. No size is returned, the
application should either know what size the data is (e.g a
structure or fixed sized array), or arrange for the data to be
self-sized (e.g. a zero terminated string or contains a size field).
The function cyg_flashsafe_read() performs a
similar job to cyg_flashsafe_data() except
that the data is copied out of the flash memory. The
data argument points to a buffer into which
the data will be copied, and the len points
to a location where the size of the buffer is stored when the call
is made, and will contain the size of data copied in on
return. This function is useful where it is intended to update the
data read from the flashsafe, possibly to write it back to
flashsafe. cyg_flashsafe_data() is useful
where the data only needs to be read, and saves valuable RAM
space.
To open a flashsafe block for update the function
cyg_flashsafe_open() should be called. This
will select the oldest block in the safe, erase it and prepare it
for writing.
The function cyg_flashsafe_write() is used to
write new data to the current open block. The
key argument should be an application
selected 16 bit value that is used to identify this data
item. This value should be unique for each item, otherwise the
behaviour is undefined. The data and
len arguments describe a buffer containing
the data to be written.
The function cyg_flashsafe_commit() causes
the current open block to be committed to the flash. This involves
calculating the checksum and writing the header and trailer with
the current sequence number.
Each of these functions may return one of a number of error codes. These may include the following:
This is returned when the operation succeeded.
This is returned when the flash device failed to initialize.
This is returned when there is a mismatch between the size any layout of the flashsafe described in the initialized cyg_flashsafe structure and the flashsafe found in flash.
This is returned when the flash driver reports a programming error.
This is returned when the flash driver reports a block erase error.
This is returned when there is no current valid block in the flashsafe. This will usually only happen when the flashsafe is new.
This is returned when a given key cannot be found in the flashsafe.
This is returned when a
cyg_flashsafe_write() or
cyg_flashsafe_commit() are called before
making a call to cyg_flashsafe_open().
This is returned when the size of data is too large for either the buffer or the flashsafe block as a whole.
The function cyg_flashsafe_errmsg(), if given
one of these error codes, will return a string describing the
error.