tcp_arg()
Name
tcp_arg() -- Set the application connection state
Synopsis
void tcp_arg(struct tcp_pcb *pcb, void *arg);
Description
The tcp_arg() function specifies the program specific
state that should be passed to all other callback functions. The "pcb"
argument is the current TCP connection control block, and the "arg"
argument is the argument that will be passed to the callbacks.