tcp_bind()
Name
tcp_bind() -- Bind PCB to local IP address and port
Synopsis
err_t tcp_bind(struct tcp_pcb *pcb, struct ip_addr *ipaddr, u16_t port);
Description
Binds pcb to a local IP address and port number. The
IP address can be specified as IP_ADDR_ANY in order to
bind the connection to all local IP addresses.
Return value
If another connection is bound to the same port, the function will return
ERR_USE, otherwise ERR_OK is
returned.