Application polling

Table of Contents
tcp_poll() -- Set application poll callback

When a connection is idle (i.e., no data is either transmitted or received), lwIP will repeatedly poll the application by calling a specified callback function. This can be used either as a watchdog timer for killing connections that have stayed idle for too long, or as a method of waiting for memory to become available. For instance, if a call to tcp_write() has failed because memory wasn't available, the application may use the polling functionality to call tcp_write() again when the connection has been idle for a while.