Allocates buffer memory with size number of bytes for
the netbuf buf. The function returns a pointer to the
allocated memory. Any memory previously allocated to the netbuf
buf is deallocated. The allocated memory can later be
deallocated with the netbuf_free()
function. Since protocol headers are expected to precede the data when it
should be sent, the function allocates memory for protocol headers as well
as for the actual data.