netconn_peer()
Name
netconn_peer() -- Obtain the remote host IP address/port of a netconn
Synopsis
err_t netconn_peer(struct netconn *conn, struct ip_addr *addr, u16_t *port);
Description
This function is used to obtain the IP address and port of the remote end of
the connection indicated by conn. The parameters
addr and port are result
parameters that are set by the function. If the connection
conn is not connected to any remote host, the results
are undefined.