netconn_type()

Name

netconn_type() -- Obtain the type of netconn

Synopsis

enum netconn_type netconn_type(struct netconn *conn);

Description

Returns the type of the connection conn. This is the same type that is given as an argument to netconn_new() (and its variants) and can be one of NETCONN_TCP, NETCONN_UDP, NETCONN_UDPLITE, NETCONN_UDPNOCHKSUM or NETCONN_RAW.