Chapter 9. Tests and utilities

Table of Contents
Unit and functional tests
Ancillary NAND utilities

Unit and functional tests

The NAND library includes a number of tests. The most useful to driver writers are readwrite, rwbenchmark and sweccwalk; the others are only likely to be of interest to library maintainers.

readwrite

Performs a read-write-erase cycle on the first NAND device it finds, checking that its operations have had the expected effect on the device contents. This is a potentially destructive test; do not run it on a device containing data you care about!

rwbenchmark

A more involved version of readwrite, this is a timing test which performs multiple reads, writes and erases and applies statistical techniques to the results in the same way that tm_basic instruments the speed of various eCos kernel functions. This is a potentially destructive test; do not run it on a device containing data you care about!

sweccwalk

Repeatedly makes single-bit changes to a data buffer and checks that the software ECC implementation correctly repairs them.

Tip: This test can be adapted to test out hardware ECC implementations. The test outputs the raw ECC codes as it goes, which is useful in confirming that the bits in the computed ECC are what you think they are.

nandunit

Some unit tests which do not require any NAND device: ECC known answer vectors, and OOB area packing/unpacking correctness.

readlimits

Attempts to read a block outside of a partition, confirming that it doesn't work.

There are some further tests of the library which require the synthetic NAND device.