The eCos kernel implements the functionality used by the µITRON compatibility subsystem. The configuration of the kernel influences the behavior of µITRON programs.
In particular, the default configuration has time slicing (also known as round-robin scheduling) switched on; this means that a task can be moved from RUN state to READY state at any time, in order that one of its peers may run. This is not strictly conformant to the µITRON specification, which states that timeslicing may be implemented by periodically issuing a rot_rdq(0) call from within a periodic task or cyclic handler; otherwise it is expected that a task runs until it is pre-empted in consequence of synchronization or communication calls it makes, or the effects of an interrupt or other external event on a higher priority task cause that task to become READY. To disable timeslicing functionality in the kernel and µITRON compatibility environment, please disable the CYGSEM_KERNEL_SCHED_TIMESLICE configuration option in the kernel package. A description of kernel scheduling is in Kernel Overview.
For another example, the semantics of task queueing when waiting on a synchronization object depend solely on the way the underlying kernel is configured. As discussed above, the multi-level queue scheduler is the only one which is µITRON compliant, and it queues waiting tasks in FIFO order. Future releases of that scheduler might be configurable to support priority ordering of task queues. Other schedulers might be different again: for example the bitmap scheduler can be used with the µITRON compatibility layer, even though it only allows one task at each priority and as such is not µITRON compliant, but it supports only priority ordering of task queues. So which queueing scheme is supported is not really a property of the µITRON compatibility layer; it depends on the kernel.
In this version of the µITRON
compatibility layer, the calls to disable and enable scheduling
and interrupts (dis_dsp(),
ena_dsp(), loc_cpu()
and unl_cpu())
call underlying kernel functions; in particular, the xxx_dsp() functions
lock the scheduler entirely, which prevents dispatching of DSRs; functions
implemented by DSRs include clock counters and alarm timers. Thus time “stops” while
dispatching is disabled with dis_dsp().
Like all parts of the eCos system, the detailed semantics of the µITRON layer are dependent on its configuration and the configuration of other components that it uses. The µITRON configuration options are all defined in the file pkgconf/uitron.h, and can be set using the configuration tool or editing the .ecc file in your build directory by hand.
An important configuration option for the µITRON compatibility layer is “Option: Return Error Codes for Bad Params” ( CYGSEM_UITRON_BAD_PARAMS_RETURN_ERRORS ), which allows a lot of the error checking code in the µITRON compatibility layer to be removed. Of course this leaves a program open to undetected errors, so it should only be used once an application is fully debugged and tested. Its benefits include reduced code size and faster execution. However, it affects the API significantly, in that with this option enabled, bad calls do not return errors, but cause an assert failure (if that is itself enabled) or malfunction internally. There is discussion in more detail about this in each section below.
We now give a brief description of the µITRON functions which are implemented in this release. Note that all C and C++ source files should have the following #include statement:
#include <cyg/compat/uitron/uit_func.h> |