#include <cyg/kernel/kapi.h>
|
void cyg_exception_set_handler(cyg_code_t exception_number, cyg_exception_handler_t* new_handler, cyg_addrword_t new_data, cyg_exception_handler_t** old_handler, cyg_addrword_t* old_data);
void cyg_exception_clear_handler(cyg_code_t exception_number);
void cyg_exception_call_handler(cyg_handle_t thread, cyg_code_t exception_number, cyg_addrword_t exception_info);
Sometimes code attempts operations that are not legal on the current hardware, for example dividing by zero, or accessing data through a pointer that is not properly aligned. When this happens the hardware will raise an exception. This is very similar to an interrupt, but happens synchronously with code execution rather than asynchronously and hence can be tied to the thread that is currently running.
The exceptions that can be raised depend very much on the hardware, especially the processor. The corresponding documentation should be consulted for more details. Alternatively the architectural HAL header file hal_intr.h, or one of the variant or platform header files it includes, will contain appropriate definitions. The details of how to handle exceptions, including whether or not it is possible to recover from them, also depend on the hardware.
Exception handling is optional, and can be disabled through the configuration option CYGPKG_KERNEL_EXCEPTIONS. If an application has been exhaustively tested and is trusted never to raise a hardware exception then this option can be disabled and code and data sizes will be reduced somewhat. If exceptions are left enabled then the system will provide default handlers for the various exceptions, but these do nothing. Even the specific type of exception is ignored, so there is no point in attempting to decode this and distinguish between say a divide-by-zero and an unaligned access. If the application installs its own handlers and wants details of the specific exception being raised then the configuration option CYGSEM_KERNEL_EXCEPTIONS_DECODE has to be enabled.
An alternative handler can be installed using
cyg_exception_set_handler. This requires a code
for the exception, a function pointer for the new exception handler,
and a parameter to be passed to this handler. Details of the
previously installed exception handler will be returned via the
remaining two arguments, allowing that handler to be reinstated, or
null pointers can be used if this information is of no interest. An
exception handling function should take the following form:
void
my_exception_handler(cyg_addrword_t data, cyg_code_t exception, cyg_addrword_t info)
{
…
}
|
The data argument corresponds to the new_data
parameter supplied to cyg_exception_set_handler.
The exception code is provided as well, in case a single handler is
expected to support multiple exceptions. The info
argument will depend on the hardware and on the specific exception.
cyg_exception_clear_handler can be used to
restore the default handler, if desired. It is also possible for
software to raise an exception and cause the current handler to be
invoked, but generally this is useful only for testing.
By default the system maintains a single set of global exception
handlers. However, since exceptions occur synchronously it is
sometimes useful to handle them on a per-thread basis, and have a
different set of handlers for each thread. This behaviour can be
obtained by disabling the configuration option
CYGSEM_KERNEL_EXCEPTIONS_GLOBAL. If per-thread
exception handlers are being used then
cyg_exception_set_handler and
cyg_exception_clear_handler apply to the current
thread. Otherwise they apply to the global set of handlers.
| Caution |
In the current implementation
|
Note: Exceptions at the eCos kernel level refer specifically to hardware-related events such as unaligned accesses to memory or division by zero. There is no relation with other concepts that are also known as exceptions, for example the throw and catch facilities associated with C++.
If the system is configured with a single set of global exception
handlers then
cyg_exception_set_handler and
cyg_exception_clear_handler may be called during
initialization or from thread context. If instead per-thread exception
handlers are being used then it is not possible to install new
handlers during initialization because the functions operate
implicitly on the current thread, so they can only be called from
thread context. cyg_exception_call_handler should
only be called from thread context.