Typical schedulers use the concept of a thread priority to determine which thread should run next. Exactly what this priority consists of will depend on the scheduler, but a typical implementation would be a small integer in the range 0 to 31, with 0 being the highest priority. Usually only the idle thread will run at the lowest priority. The exact number of priority levels available depends on the configuration, typically the option CYGNUM_KERNEL_SCHED_PRIORITIES.
cyg_thread_get_priority can be used to determine
the priority of a thread, or more correctly the value last used in a
cyg_thread_set_priority call or when the thread
was first created. In some circumstances it is possible that the
thread is actually running at a higher priority. For example, if it
owns a mutex and priority ceilings or inheritance is being used to
prevent priority inversion problems, then the thread's priority may
have been boosted temporarily.
cyg_thread_get_current_priority returns the real
current priority.
In many applications appropriate thread priorities can be determined
and allocated statically. However, if it is necessary for a thread's
priority to change at run-time then the
cyg_thread_set_priority function provides this
functionality.