This is a port of UCD-SNMP-4.1.2
Originally this document said: See http://ucd-snmp.ucdavis.edu/ for details. And send them a postcard.
The project has since been renamed “net-snmp” and re-homed at http://net-snmp.sourceforge.net/ where various new releases (of the original, not eCos ports) are available.
The original source base from which we worked to create the eCos port is available from various archive sites such as ftp://ftp.freesnmp.com/mirrors/net-snmp/ generally with this filename and details:
ucd-snmp-4.1.2.tar.gz. . . . . . Nov 2 2000 1164k |