2007-10-10  Nick Garnett  <nickg@ecoscentric.com>

	* src/if_dm9000.c (db_printf): Improved debug facilities.
	(eeprom_read, eeprom_write, dm9000_init, dm9000_ioctl): Disable
	EEPROM support; currently permanently.

2005-11-07  David Vrabel <dvrabel@arcom.com>

	* src/if_dm9000.c, include/dm9000_info.h: Support interrupts.
	* cdl/davicom_dm9000_eth_drivers.cdl
	(CYGPKG_DEVS_ETH_DAVICOM_DM9000_CFLAGS_ADD): Need _KERNEL and
	__ECOS defined for non-stand-alone builds.

2005-10-25  David Vrabel <dvrabel@arcom.com>

	* src/if_dm9000.c (eeprom_read, eeprom_write, eeprom_reload):
	Delay more when writing/reading eeprom (200 us isn't enough).
	(phy_init): Turn on PHY before writing PHY registers.  Wait for
	auto negotiation to be complete.
	(dm9000_send): Correctly write last words to Tx SRAM when using a
	8/16 bit device.  Clarify and comment code.
	(dm9000_poll): Parse Rx packet header correctly on 8/16 bit
	devices.
	(dm9000_ioctl): Handle ETH_DRV_GET_MAC_ADDRESS and
	ETH_DRV_SET_MAC_ADDRESS.

	* cdl/davicom_dm9000_eth_drivers.cdl: New option
	CYGSEM_DEVS_ETH_DAVICOM_DM9000_WRITE_EEPROM to enable/disable
	writing to EEPROM.

2004-09-05  Mark Salter <msalter@redhat.com>

	Initial Checkin of DM9000 Ethernet driver (RedBoot only for now).

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================