2009-04-21  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c: fix a couple of typos

2008-11-17  Bart Veer  <bartv@ecoscentric.com>

	* cdl/mcf5272.cdl, doc/mcf5272_eth.sgml, src/if_mcf5272.c: minor
	clean-ups.

2008-09-22  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c (mcf52xx_eth_deliver): avoid cpp warning when
	building for processors without a data cache.

2008-09-02  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c, (mcf52xx_eth_init): add
	support for run-time device dection.

2008-06-02  Bart Veer  <bartv@ecoscentric.com>

	* cdl/mcf5272_eth.cdl: add constraints so net tests run with
	sensible performance.

2008-03-18  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c: rearrange RX interrupt masking to avoid
	spurious interrupt exceptions.

2008-03-03  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c: encapsulate stats gathering in a macro.

2008-02-28  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c: cleanup and more coping with unified and
	copyback caches.

	* cdl/mcf5272_eth.cdl: the ethernet driver must be built with at
	least -O1 to ensure some data stays in registers when manipulating
	the cache.

2008-02-14  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c: cope with unified and copyback caches.

2007-04-25  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/mcf5272_eth.cdl: memset/memcpy are part of infra and always
	declared in isoinfra, so don't need to require CYGPKG_LIBC_STRING.
	Require CYGPKG_ISOINFRA instead, although that's in every template
	anyway.

2006-09-25  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c: remove unnecessary #error

	* cdl/mcf5272_eth.cdl, src/if_mcf5272, doc/mcf5272_eth.sgml:
	Motorola -> Freescale.

2006-09-08  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c: more/enhanced diagnostics. Update to use
	current var_io.h definitions. Add partial support for multiple
	devices.

2006-03-10  John Dallaway  <jld@ecoscentric.com>

	* cdl/mcf5272_eth.cdl: Add reference to package documentation.

2004-10-07  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c (mcf52xx_eth_init): add optional platform init
	function

2004-06-25  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c (DEBUG): add some debug/tracing support

2004-05-20  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c, cdl/mcf5272_eth.cdl: add a dependency
	on CYGPKG_LIBC_STRING to get memcpy()

2004-04-21  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c (mcf52xx_eth_init): use the right macro if the
	platform has its own way of supplying a MAC address.

2004-03-25  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c (mcf52xx_eth_deliver): make the rx ring scan
	more robust. The mcf5282 appears to occasionally place incoming
	frames in unexpected slots.

2004-03-17  Bart Veer  <bartv@ecoscentric.com>

	* doc/mcf5272_eth.sgml: update documentation following port to an
	mcf5282

2004-03-10  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c (mcf52xx_eth_poll): update tx poll code to
	match previous changes. Ignore the MAC address passed to _start(),
	it is not needed. During _init(), if running on top of RedBoot,
	check for an outgoing transmit before resetting and wait a bit if
	necessary.

2004-03-08  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c: cope with processor variants where tx buffers
	need to be more aligned than is guaranteed by higher-level code.
	Provide a MAC address even if virtual vectors are not available,
	e.g. when debugging via BDM. Reorganize the init code as per the
	recommendations in the mcf5282 manual. Add statistics counting for
	the mcf5282. Disable RX interrupts between the ISR and the
	received packet(s) being processed, since those just add to the
	load. Use separate ISR priorities for RX and TX.

	* cdl/mcf5272_eth.cdl: At least two rx buffers are needed to cope
	with oversized incoming frames. ISR priorities now have to be
	configured separately for RX and TX.

2004-02-11  Bart Veer  <bartv@ecoscentric.com>

	* src/if_mcf5272.c: The driver now works on coldfire processors
	other than just the 5272. Use new per-processor initialization
	macro to set up GPIO pins. Also cope with incompatible renaming
	of flash configury within hal/common.

	* cdl/mcf5272_eth.cdl: update descriptions to reflect that the
	driver now works on other coldfire processors as well.

2003-07-22  Bart Veer  <bartv@ecoscentric.com>

	* doc/mcf5272_eth.sgml: fix various typos etc

	* src/if_mcf5272.c (mcf5272_eth_deliver): eliminate warning

	* cdl/mcf5272_eth.cdl: RedBoot now needs more than one buffer.

2003-07-18  Bart Veer  <bartv@ecoscentric.com>

	* doc/mcf5272_eth.sgml: add documentation

2003-07-13  Bart Veer  <bartv@ecoscentric.com>

	* cdl/mcf5272_eth.cdl:
	Increase default number of receive buffers.

	* src/if_mcf5272.c:
	Implement SNMP statistics
	Improve handling of overrun conditions
	Preserve order of incoming packets

2003-06-04  Bart Veer  <bartv@ecoscentric.com>

	* New version of the M68K support

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2003, 2004, 2007, 2008 Free Software Foundation, Inc.      
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================