2008-11-17  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/flash_atmel_at29cxxxx.cdl: Indicate that this driver uses
	the legacy flash device API.

2003-01-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/flash_at29cxxxx.inl: Fix truncated codes for 16-bit
	AT29LV1024.
	Allow FLASH_NUM_REGIONS and CYGNUM_FLASH_BASE_MASK to be overridden.
	(flash_hwr_init): set flash_info.block_mask.
	(flash_query): increase delay.
	(flash_erase_block): use CYGNUM_FLASH_BASE_MASK. Correct previous
	change from Roland which may have worked for 2*8-bit devices, but
	broke single 16-bit devices.
	(flash_program_buf): Ditto.	

2003-10-02  Roland Cassebohm  <r.cassebohm@visionsystems.de>

	* include/flash_at29cxxxx.inl: Improves driver, to work with 16 bit
	wide access. The driver have to write 256 times after each command 
	sequence, but with two 8 bit divices parallel, the driver writes
	only 128 times.

2001-09-13  Jesper Skov  <jskov@redhat.com>

	* include/flash_at29cxxxx.inl: Added support for AT29LV1024. Added
	code to erase blocks. Made driver work with 16bit wide
	parts. Fixed flash size calculations.

2001-05-23  Jesper Skov  <jskov@redhat.com>

	* cdl/flash_atmel_at29cxxxx.cdl: Links functions to RAM. IO driver
	need not copy.

2001-02-23  Jesper Skov  <jskov@redhat.com>

	* include/flash_at29cxxxx.inl: Include type macros from IO driver.

2001-02-22  Jesper Skov  <jskov@redhat.com>

	* include/flash_at29cxxxx.inl: Moved flash_query function. Call it
	indirectly through the IO driver.

2001-02-20  Jesper Skov  <jskov@redhat.com>

	* .../atmel/at29cxxxx: Cloned from am29xxxxx driver.

2000-12-07  Jesper Skov  <jskov@redhat.com>

	* src/flash.h: Addresses and sizes are also affected by
	interleaving.
	* src/flash_erase_block.c: Plug in working loop.
	* src/flash_program_buf.c: Same.

2000-12-06  Jesper Skov  <jskov@redhat.com>

	* src/am29f040b_flash.c (flash_hwr_init): Use new query semantics.
	* src/flash_query.c (flash_query): Changed accordingly.

	* src/flash.h (FLASH_Sector_Erase_Timer): Added.

	* src/flash_erase_block.c: Do not check error flag after operation
	completes.
	* src/flash_program_buf.c: Same.

2000-12-05  Jonathan Larmour  <jlarmour@redhat.com>

	* src/am29f040b_flash.c (flash_code_overlaps): Define stext/etext
	as array types so no assumptions can be made by the compiler about
	location.

2000-12-05  Jesper Skov  <jskov@redhat.com>

	* Cloned from MBX driver.

2000-10-20  Gary Thomas  <gthomas@redhat.com>

	* src/mbx_flash.c: 
	* src/flash_query.c: 
	* src/flash_program_buf.c: 
	* src/flash_erase_block.c: 
	* src/flash.h: 
	* cdl/flash_mbx.cdl: New package/file(s).

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004 Free Software Foundation, Inc.
// Copyright (C) 2004 eCosCentric Limited                                   
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================