2008-12-23   Evgeniy Dushistov <dushistov@mail.ru>
	
	* include/flash_at49xxxx_parts.inl: Add support for
	AT49BV642D.
	
2008-11-17  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/flash_atmel_at49xxxx.cdl: Indicate that this driver uses
	the legacy flash device API.

2005-02-15  Jacques Tinembart <Jacques.Tinembart@eig.unige.ch>
 
 	* include/flash_at49xxxx.inl, include/flash_at49xxxx_parts.inl:
 	add support for AT49LV161 and AT49BV322A
 
2004-11-12  Andrew Lunn  <andrew.lunn@ascom.ch>

	* include/flash_at49xxxx_parts.inl: Give a compiler error if the
	bug workaround for the AT49BV16[01]4A is not enabled.

2004-09-30  Savin Zlobec <savin@elatec.si>

	* cdl/flash_atmel_at49xxxx.cdl: Fixed typo in
	CYGHWR_IO_FLASH_DEVICE_LEGACY.

2004-05-11  Thomas Koeller  <thomas.koeller@baslerweb.com>

	* cdl/flash_atmel_at49xxxx.cdl:
	* include/flash_at49xxxx.inl: Added workaround for Atmel
	AT91FR40162 erase bug.

2003-11-10  Gary Thomas  <gary@mlbassoc.com>

	* include/flash_at49xxxx_parts.inl: Add AT29LV200BB

2003-09-19  Gary Thomas  <gary@mlbassoc.com>

	* include/flash_at49xxxx_parts.inl: Add support for AT49LV040

	* include/flash_at49xxxx.inl: Support devices which need "chip erase"
	as opposed to "sector erase" operations.

2003-08-08  Oyvind Harboe <oyvind.harboe@zylin.com>

	* include/flash_at49xxxx.inl: the program/erase completion had a
	race condtion.  Changes algorithms to one that does not suffer
	from potential race conditions.

2003-07-15  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/flash_at49xxxx.inl: Reorganise to support boot blocks,
	multiple flash types from the same driver, and do proper
	verification.
	* include/flash_at49xxxx_parts.inl: New file to describe flash
	part information.

2003-06-10  Øyvind Harboe  <oyvind.harboe@zylin.com>

	* include/flash_at49xxxx.inl: wait_while_busy needs to be in RAM
	since its called while the flash is not readable.
	
2002-07-12  Tim Drury (tdrury@siliconmotorsports.com>

	* include/flash_at49xxxx.inl: added support for AT49LV1614

2002-06-24  Jani Monoses <jani@iv.ro>

	* include/flash_at49xxxx.inl: Added support for AT49BV8011
	based on AT29XXXXX
	
//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================