2006-12-21  Wang Cui <iucgnaw@msn.com>

	* include/flash_sst_39vfxxx.inl: Add supported devices:
	SST39VF160, SST39VF1601, SST39VF1602, SST39VF320, SST39VF3201,
	SST39VF3202, SST39VF6401, SST39VF6402,

2006-08-02  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/flash_sst_39vfxxx.inl: In CYG_FLASH_FUNS, replace lock
	and unlock functions with generic nop versions.
	Remove hwr_map_error: it no longer exists for CYG_FLASH_FUNS.

2004-11-29  Bart Veer  <bartv@ecoscentric.com>

	* include/flash_sst_39vfxxx.inl: eliminate hwr_map_error(), no
	longer needed by the generic flash code.
	* include/flash_sst_39vfxxx.inl: use the dummy lock/unlock
	functions provided by the generic flash code.

2004-11-25  Bart Veer  <bartv@ecoscentric.com>

	* cdl/flash_sst_39vfxxx.cdl: this V2 driver relies on the generic
	flash code to handle the cache

2004-11-22  Bart Veer  <bartv@ecoscentric.com>
	
	* include/flash_sst_39vfxxx.inl: assume static initialization and
	adjust const's in various parameters
	* include/flash_sst_39vfxxx.inl: rename cyg_block_info to
	cyg_flash_block_info

2004-09-14  Andrew Lunn  <andrew.lunn@ascom.ch>

	* include/flash_sst_39vfxxx.inl: Set the end address to the last
	valid address in flash, not the first invalid address.

2004-08-06  Andrew Lunn  <andrew.lunn@ascom.ch>

	* include/flash_sst_39vfxxx.inl: The structure declared by
	CYG_FLASH_FUNS should be static so we can instantiate the
	driver multiple times.

2004-08-04  Andrew Lunn  <andrew.lunn@ascom.ch>

	* include/flash_sst_39vfxxx.inl: Added support for the SST39VF160
	device.

2004-07-16  Andrew Lunn  <andrew.lunn@ascom.ch>

	* include/flash_sst_39vfxxx.inl: Modified the driver to make use
	of the new flash device API.

2003-10-02  Roland Caßebohm <r.cassebohm@visionsystems.de>

	* include/flash_sst_39vfxxx.inl: 
	* cdl/flash_sst_39vfxxx.cdl: New package cloned from at29xxxx driver.
	Supported devices: SST39VF080, SST39VF016 and SST39VF400.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2006 Free Software Foundation, Inc.
// Copyright (C) 2006 eCosCentric Limited                                   
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================