2009-11-13  Ross Younger  <wry@ecoscentric.com>

	* Don't provide bbt_data if it isn't called for.

2009-11-09  Ross Younger  <wry@ecoscentric.com>

	* Driver update: add read_part_page function.

2009-11-06  Ross Younger  <wry@ecoscentric.com>

	* nand_st_xxxx3a.sgml: Remove link to cortexm hal.

2009-10-19  Ross Younger  <wry@ecoscentric.com>

	* Update to driver v2. Require CYGSEM_IO_NAND_INTERFACE_VERSION >= 2.

2009-08-11  Ross Younger  <wry@ecoscentric.com>

	* Improve driver timings, sundry tidyups

2009-06-30  Simon Kallweit  <simon.kallweit@intefo.ch>

	* New package. ST Microelectronics NANDxxxx3A flash chips.

//===========================================================================
// ####ECOSGPLCOPYRIGHTBEGIN####                                            
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2009 Free Software Foundation, Inc.
//
// eCos is free software; you can redistribute it and/or modify it under    
// the terms of the GNU General Public License as published by the Free     
// Software Foundation; either version 2 or (at your option) any later      
// version.                                                                 
//
// eCos is distributed in the hope that it will be useful, but WITHOUT      
// ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or    
// FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public License    
// for more details.                                                        
//
// You should have received a copy of the GNU General Public License        
// along with eCos; if not, write to the Free Software Foundation, Inc.,    
// 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301, USA.            
//
// As a special exception, if other files instantiate templates or use      
// macros or inline functions from this file, or you compile this file      
// and link it with other works to produce a work based on this file,       
// this file does not by itself cause the resulting work to be covered by   
// the GNU General Public License. However the source code for this file    
// must still be made available in accordance with section (3) of the GNU   
// General Public License v2.                                               
//
// This exception does not invalidate any other reasons why a work based    
// on this file might be covered by the GNU General Public License.         
// -------------------------------------------                              
// ####ECOSGPLCOPYRIGHTEND####                                              
//===========================================================================