2009-03-05  Bart Veer  <bartv@ecoscentric.com>

	* src/wallclock_at91.cxx: update init priorities.

2006-07-11  Nick Garnett  <nickg@ecoscentric.com>

	* src/wallclock_at91.cxx (rtc_isr): Added some missing parentheses
	which were triggering CYG_FAIL() unexpectedly.

2006-07-10  Nick Garnett  <nickg@ecoscentric.com>

	* src/wallclock_at91.cxx: Fixed bug in condition variable
	declaration.

2006-07-06  Nick Garnett  <nickg@ecoscentric.com>

	* src/wallclock_at91.cxx: Fixed some synchronization issues.

2005-12-12  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/wallclock_at91.cxx (arm_global_ints_are_on): Use
	HAL_QUERY_INTERRUPTS() rather than having a disable.

2005-09-14  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/wallclock_at91.cdl: Of the AT91 (not AT91RM9200) family, only
	AT91M55800A has an RTC so far.

	* src/wallclock_at91.cxx: Support AT91 naming of various defines.

2005-08-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* New package. Support for on-chip RTC of Atmel AT91 and AT91RM9200
	CPUs.

// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2005, 2009 eCosCentric Limited                                   
// Copyright (C) 2005 Free Software Foundation, Inc.                        
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####