2008-04-24  John Dallaway  <jld@ecoscentric.com>

	* cdl/watchdog_lpc2xxx.cdl,
	  src/watchdog_lpc2xxx.cxx: "Philips" -> "NXP".

2008-03-10  Nick Garnett  <nickg@ecoscentric.com>

	* src/watchdog_lpc2xxx.cxx (start): Add initialization of WDCLKSEL
	register if it is defined.

2008-02-05  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/watchdog_lpc2xxx.cxx (wdint): Ensure this is initialised at
	the correct init priority, otherwise the contents are not set up
	before they are used by watchdog constructor.

2005-05-20  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/watchdog_lpc2xxx.cxx (WD_TIMER_CONSTANT_INIT): Timer constant
	was calculating wd ticks to wait for the number of microseconds,
	not seconds as it should have been.

2004-08-18  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/watchdog_lpc2xxx.cxx (start): Don't clear WDTOF with 1.
	Use WDEN even when intending to reset.

2004-08-05  Jonathan Larmour  <jifl@eCosCentric.com>

	* New package. Support for on-board watchdog for Philips LPC2xxx.

// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2004, 2005, 2008 Free Software Foundation, Inc.            
// Copyright (C) 2004,2005, 2008 eCosCentric Limited                        
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####