2009-03-05  Bart Veer  <bartv@ecoscentric.com>

	* cdl/hal_arm_arm9_dnp_sk23.cdl: update compiler flags for gcc 4.x

2009-01-24  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_arm_arm9_dnp_sk23.cdl: switch from arm-elf-gcc to
	arm-eabi-gcc.

2008-05-08  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/hal_arm_arm9_dnp_sk23.cdl: We now support MMC/SD again.
	* doc/dnp_sk23.sgml: Update docs for new SD support, and impact
	of no card detection, or write protect switch sampling.
	* include/plf_io.h: Provide platform defines for updated
	MMC/SD driver.

2008-04-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/hal_arm_arm9_dnp_sk23.cdl: Disable claimed MMC support
	until platform support revised for updated AT91RM9200 MCI
	driver.

2007-09-12  John Dallaway  <jld@ecoscentric.com>

	* doc/dnp_sk23.sgml: Remove unwanted whitespace which affects
	formatting.

2007-09-11  Nick Garnett  <nickg@ecoscentric.com>

	* include/hal_platform_setup.h: Set PA22-23 to peripheral A for
	UART2.

	* cdl/hal_arm_arm9_dnp_sk23.cdl: Add UART2 support. Limit comm
	channel count to 2.

2007-09-11  John Dallaway  <jld@ecoscentric.com>

	* misc/redboot_ROMRAM.ecm, misc/redboot_ROM.ecm: Add wallclock I/O
	package.

	* misc/redboot_UBOOT.ecm: Correct CYGBLD_REDBOOT_MIN_IMAGE_SIZE.

	* doc/dnp_sk23.sgml: Fix RedBoot JTAG download address and add
	instructions for Kermit download via U-Boot.

2007-09-10  John Dallaway  <jld@ecoscentric.com>

	* sgml/dnp_sk23.sgml: Fix duplicate refsect1 ID. Reference DNP/EVA9
	evaulation board.

2006-12-19  John Dallaway  <jld@ecoscentric.com>

	* misc/redboot_ROMRAM_RBL.ecm: Remove.
	* sgml/dnp_sk23.sgml: Reflect the above change.

2006-12-18  John Dallaway  <jld@ecoscentric.com>

	* cdl/hal_arm_arm9_dnp_sk23.cdl: Reference package documentation.

2006-11-23  John Dallaway  <jld@ecoscentric.com>

	* cdl/hal_arm_arm9_dnp_sk23.cdl: Allow CYGBLD_BUILD_REDBOOT_WITH_EXEC
	to be disabled.

2006-10-10  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_arm_arm9_dnp_sk23.cdl: Change serial device interface
	names in line with AT91RM9200 HAL.

	* doc/dnp_sk23.sgml: Update to reflect changes in UART to device
	mapping.

2006-08-02  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/dnp_sk23_flash.c: In CYG_FLASH_FUNS, replace query function
	with generic nop version.
        Remove hwr_map_error: it no longer exists for CYG_FLASH_FUNS.

2006-06-19  Nick Garnett  <nickg@ecoscentric.com>

	* misc/redboot_JTAG.ecm:	
	* misc/redboot_RAM.ecm: 
	* misc/redboot_ROM.ecm: 
	* misc/redboot_ROMRAM.ecm: 
	* misc/redboot_ROMRAM_RBL.ecm: 
	* misc/redboot_UBOOT.ecm: Minor edits.

	* misc/redboot_JTAG.ecm:
	Add CYGBLD_HAL_ARM9_DNP_SK23_LOAD_LOW_RAM to force low memory
	loading.

	* include/pkgconf/mlt_arm9_dnp_sk23_rom.ldi: 
	* include/pkgconf/mlt_arm9_dnp_sk23_romram.ldi: 
	* include/pkgconf/mlt_arm9_dnp_sk23_low_ram.ldi: 
	* include/pkgconf/mlt_arm9_dnp_sk23_low_ram.h:
	Updated load address, it clashed with the MMU table.

	* src/dnp_sk23_flash.c: Fix bug in flash address specification.

	* doc/dnp_sk23.sgml: Updated documentation.

2006-06-05  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_arm_arm9_dnp_sk23.cdl:
	* include/dnp_sk23-eth.inl:
	* include/dnp_sk23.h:
	* include/hal_diag.h:
	* include/hal_platform_setup.h:
	* include/plf_io.h:
	* include/plf_stub.h:
	* include/pkgconf/mlt_arm9_dnp_sk23_jtag.h:
	* include/pkgconf/mlt_arm9_dnp_sk23_jtag.ldi:
	* include/pkgconf/mlt_arm9_dnp_sk23_ram.h:
	* include/pkgconf/mlt_arm9_dnp_sk23_ram.ldi:
	* include/pkgconf/mlt_arm9_dnp_sk23_rom.h:
	* include/pkgconf/mlt_arm9_dnp_sk23_rom.ldi:
	* include/pkgconf/mlt_arm9_dnp_sk23_romram.h:
	* include/pkgconf/mlt_arm9_dnp_sk23_romram.ldi:
	* include/pkgconf/mlt_arm9_dnp_sk23_uboot.h:
	* include/pkgconf/mlt_arm9_dnp_sk23_uboot.ldi:
	* misc/bdi2000.dnp_sk23.cfg:
	* misc/redboot_JTAG.ecm:
	* misc/redboot_RAM.ecm:
	* misc/redboot_ROM.ecm:
	* misc/redboot_ROMRAM.ecm:
	* misc/redboot_ROMRAM_RBL.ecm:
	* src/dnp_sk23_flash.c:
	* src/dnp_sk23_misc.c:
	New package -- support for SSV DNP/SK23 board.

	* doc/dnp_sk23.sgml: 
	This is currently a stright copy of the ATMEL-AT91RM9200-KITS
	documentation, pending reorganization of AT91RM9200
	documentation.
	
//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2005, 2006, 2007, 2008 Free Software Foundation, Inc.      
// Copyright (C) 2005, 2006, 2007, 2008 eCosCentric Limited                 
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================