2009-03-05  Bart Veer  <bartv@ecoscentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl: update compiler flags for gcc
	4.x

2009-01-24  Bart Veer <bartv@ecoscentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl: switch from arm-elf-gcc to
	arm-eabi-gcc.

2008-12-05  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl: Add configuration for LPC2xxx
	internal flash.

	* include/pkgconf/mlt_arm_phycore_ram.h:
	* include/pkgconf/mlt_arm_phycore_ram.ldi:
	* include/pkgconf/mlt_arm_phycore_rom.h:
	* include/pkgconf/mlt_arm_phycore_rom.ldi: Add definitions for
	internal SRAM.

	* misc/redboot_ROM.ecm: Add options to avoid use of internal flash
	for FIS and fconfig.
	
2008-12-05  John Dallaway  <jld@ecoscentric.com>

	* doc/phycore.sgml: Updated documentation for installation of RedBoot
	using Flash Magic and for updating RedBoot using RedBoot itself.

	* misc/redboot_RAM.ecm: New file to build RedBoot for RAM startup.

2008-02-05  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl: Crystal OSC frequency should
	be 10MHz, not 20MHz. Luckily since the PLL divider had previously
	been misapplied, the other values stay the same.

2006-06-30  John Dallaway  <jld@ecoscentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl: Flavor "none" for
	CYGHWR_HAL_ARM_LPC2XXX_PHYCORE_MEMORY_CONFIGURATION. Reference
	per-package documentation.

2006-06-29  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl: Added config options to define
	flash and SRAM fitted to board.

	* include/hal_platform_setup.h: Adjust SRAM timing to encompass a
	wider variety of devices.

	* include/pkgconf/mlt_arm_phycore_ram.h:
	* include/pkgconf/mlt_arm_phycore_ram.ldi:
	* include/pkgconf/mlt_arm_phycore_rom.h:
	* include/pkgconf/mlt_arm_phycore_rom.ldi:
	Use configuration options to define size of RAM.
	
	* doc/phycore.sgml: Updated documentation with options for flash
	and SRAM variations.

2006-06-16  Nick Garnett  <nickg@ecoscentric.com>

	* include/plf_io.h (HAL_AM29XXXXX_UNCACHED_ADDRESS): Added this
	macro to keep flash driver happy.

2005-07-06  Nick Garnett  <nickg@ecoscentric.com>

	* include/hal_platform_setup.h: Adjust PINSEL1 to enable use of
	CAN controllers.

2005-05-26  John Dallaway  <jld@ecoscentric.com>

	* include/hal_platform_setup.h: Adjust PINSEL0 to enable use
	of UART1.

2005-05-19  John Dallaway  <jld@ecoscentric.com>

	* doc/phycore.sgml: Clean up, note that hardware handshaking
	lines are not accessible via the HD200 board and that the
	bottom block of external Flash is reserved.

2005-05-18  John Dallaway  <jld@ecoscentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl: Eliminate SRAM startup type.
	* cdl/hal_arm_lpc2xxx_phycore.cdl: Eliminate irrelevant CDL
	option.
	* misc/redboot_RAM.ecm: Delete.
	* misc/redboot_ROM.ecm: Reserve first block of external Flash.

2005-05-16  John Dallaway  <jld@ecoscentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl: Clean up display strings.

2005-05-16  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl:
	Set CYGBLD_REDBOOT_MIN_IMAGE_SIZE to zero.

2005-05-13  Nick Garnett  <nickg@ecoscentric.com>

	* misc/redboot_RAM.ecm: 
	* misc/redboot_ROM.ecm: Removed old flash driver setting.

2005-05-12  John Dallaway  <jld@ecoscentric.com>

	* misc/redboot_ROM.ecm, misc/redboot_RAM.ecm: Enable
	CYGBLD_ARM_ENABLE_THUMB_INTERWORK.

2005-05-10  John Dallaway  <jld@ecoscentric.com>

	* doc/phycore.sgml: Make all IDs unique.

2005-04-05  John Dallaway  <jld@ecoscentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl: Eliminate
	-mno-short-load-words from the CFLAGS and LDFLAGS. It is not
	required and has been renamed for GCC 3.4.

2005-01-21  Nick Garnett  <nickg@ecoscentric.com>

	* src/phycore_misc.c (hal_platform_init): Added this function to
	handle platform-specific initialization.

	* include/hal_platform_setup.h: Re-enabled EINT0 for ethernet
	device.

2005-01-19  Nick Garnett  <nickg@ecoscentric.com>

	* include/hal_platform_setup.h: Reinstated LED macros. Disabled
	ethernet interrupt line for now. Reduced wait states on RAM, to
	give slightly better performance.

	* src/phycore_misc.c (hal_lpc2xxx_set_leds): Fixed to manipulate
	LED line correctly.

2005-01-12  Nick Garnett  <nickg@ecoscentric.com>

	* misc/redboot_ROM.ecm: Enabled ethernet options.

	* include/pkgconf/mlt_arm_phycore_ram.h: Updated to match .ldi file.

	* doc/phycore.sgml: Rewritten to document this board.

	* include/hal_platform_setup.h: Tidied up a little.

2004-11-16  Nick Garnett  <nickg@ecoscentric.com>

	* misc/redboot_ROM.ecm: Temporarily, disabled ethernet
	support. The device does not seem to be working.

2004-11-08  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/hal_arm_lpc2xxx_phycore.cdl:
	* doc/phycore.sgml:
	* include/hal_platform_ints.h:
	* include/hal_platform_setup.h:
	* include/plf_io.h:
	* include/pkgconf/mlt_arm_phycore_ram.h:
	* include/pkgconf/mlt_arm_phycore_ram.ldi:
	* include/pkgconf/mlt_arm_phycore_rom.h:
	* include/pkgconf/mlt_arm_phycore_rom.ldi:
	* include/pkgconf/mlt_arm_phycore_sram.h:
	* include/pkgconf/mlt_arm_phycore_sram.ldi:
	* misc/redboot_RAM.ecm:
	* misc/redboot_ROM.ecm:
	* src/phycore_misc.c:
	New package to support the Phytec phyCORE-LPC229X board.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2004, 2005, 2006, 2008 Free Software Foundation, Inc.      
// Copyright (C) 2004, 2005, 2006, 2008 eCosCentric Limited                 
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================