2009-04-21  Bart Veer  <bartv@ecoscentric.com>

	* include/var_intr.h: fix a couple of typos

2009-02-09  Bart Veer  <bartv@ecoscentric.com>

	* include/var_io.h (HAL_MCFxxxx_SDRAMC_DACRx_CBM_xx): fix
	definitions.

2008-11-18  Bart Veer  <bartv@ecoscentric.com>

	* whole package. Replace the original M68K port.

2008-11-17  Bart Veer  <bartv@ecoscentric.com>

	* cdl/hal_m68k_mcf52xx.cdl, doc/mcf52xx.sgml, include/hal_diag.h,
	include/var_arch.h, include/var_cache.h, include/var_intr.h,
	include/var_io.h, src/hal_diag.c, src/mcf52xx_asm.S: minor
	clean-ups.

2008-09-01  Bart Veer  <bartv@ecoscentric.com>

	* include/var_io.h (HAL_MCF52xx_QSPIx_QCRn_QSPI_CS_CSn): fix typo

2008-05-08  Bart Veer  <bartv@ecoscentric.com>

	* include/var_io.h (HAL_MCF52xx_GPTx_PORT): fix typo.

2008-03-18  Bart Veer  <bartv@ecoscentric.com>

	* include/var_io.h: add definitions for 32-bit CAN devices, PWM,
	RTC, MDHA, RNG and SKHA modules which are now common to many
	ColdFire processors.

2008-02-28  Bart Veer  <bartv@ecoscentric.com>

	* cdl/hal_m68k_mcf52xx.cdl, src/mcf52xx.c, src/mcf52xx_asm.S: add
	variant-level support for a profiling timer using an
	mcf5282-compatible PIT.

2008-02-14  Bart Veer  <bartv@ecoscentric.com>

	* include/var_io.h, include/var_intr.h: add support for interrupt
	controllers with set/clear mask registers.

2007-03-21  Nick Garnett  <nickg@ecoscentric.com>

	* include/var_intr.h (HAL_INTERRUPT_SET_LEVEL): Two-controller
	version of this macro was same as single controller version. Fixed
	to deal with two controllers.

2007-02-04  Bart Veer  <bartv@ecoscentric.com>

	* src/hal_diag.c (hal_mcf52xx_diag_uart_init): in configurations
	where the diag init code can get called multiple times, detect
	this and skip reinitializations.

2006-12-11  Bart Veer  <bartv@ecoscentric.com>

	* cdl/hal_m68k_mcf52xx.cdl: add virtual vector support for dynamic
	baud rates, for those platforms which support it.

2006-12-03  Bart Veer  <bartv@ecoscentric.com>

	* include/var_intr.h: fix support for processors with two
	interrupt controllers.

2006-10-02  John Dallaway  <jld@ecoscentric.com>

	* doc/mcf52xx.sgml: Fix minor typographical errors.

2006-09-25  Bart Veer  <bartv@ecoscentric.com>

	* doc/mcf52xx.sgml: Bring up to date following recent changes in
	M68K HALs.

2006-09-08  Bart Veer  <bartv@ecoscentric.com>

	* include/var_io.h: fix ethernet and uart definitions. Add
	QSPI_CS_CSn().

	* include/var_arch.h: fix typo

	* src/hal_diag.c, include/hal_diag.h, cdl/hal_m68k_mcf52xx.cdl:
	Sort out interaction with virtual vectors. 

2006-09-05  Bart Veer  <bartv@ecoscentric.com>

	* include/var_io.h: Use HZ rather than MHZ to calculate SPI baud
	rates. 

	* include/var_intr.h: HAL_VSR_SET() is now optional.

	* include/var_arch.h: improved versions of the LSBIT() and MSBIT()
	HAL macros.

	* src/hal_diag.c, include/hal_diag.h, cdl/hal_m68k_mcf52xx.cdl:
	Generalize HAL diagnostics support.

2006-08-22  Bart Veer  <bartv@ecoscentric.com>

	* include/var_io.h: provide definitions for most of the mcf5282
	on-chip devices, since these are now regularly encountered on
	other ColdFires so the definitions can be shared.

	* include/var_intr.h: provide default implementations of various
	interrupt/clock/reset macros for processors that have
	mcf5282-compatible on-chip devices.

	* include/var.inc: provide default implementations of
	hal_context_extract_isr_vector here instead of the processor HALs

	* src/hal_diag.c, include/hal_diag.h: generalize the diagnostics
	support, including a bitbucket option.

2006-03-10  John Dallaway  <jld@ecoscentric.com>

	* cdl/hal_m68k_mcf52xx.cdl: Add reference to MCF52xx variant
	documentation.

2005-04-15  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/hal_m68k_mcf52xx.cdl: Define a HAL variant header in
	<pkgconf/system.h>

2004-03-03  Bart Veer  <bartv@ecoscentric.com>

	* src/hal_diag.c (hal_mcf52xx_serial_control): Add support for
	RedBoot's baudrate command, if appropriate for the platform.

2004-02-11  Bart Veer  <bartv@ecoscentric.com>

	* include/var_io.h: move cacr/acr/rambar/rombar definitions to the
	processor HAL. These are not as generic as initially thought.

	* include/var.inc: make it easier for processors to override
	savestate settings.

	* doc/mcf52xx.sgml: update to reflect MCF5282 support

2003-08-01  Bart Veer  <bartv@ecoscentric.com>

	* include/var.inc: hal_context_extract_sr is no longer needed and
	has been removed.

2003-07-22  Bart Veer  <bartv@ecoscentric.com>

	* doc/mcf52xx.sgml: fix various typos etc.

2003-07-17  Bart Veer  <bartv@ecoscentric.com>

	* doc/mcf52xx.sgml: Add documentation

2003-07-08  Bart Veer  <bartv@ecoscentric.com>

	* include/var_io.h:
	Move some UART definitions to the processor HAL because they are
	not available on all MCF52xx processors

2003-06-04  Bart Veer  <bartv@ecoscentric.com>

	* New version of the M68K support

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2003, 2004, 2005, 2006, 2008 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================