2008-08-29  Nick Garnett  <nickg@ecoscentric.com>

	* cdl/httpd.cdl: Add CDL to permit the HTTP system monitor to be
	built as a loadable module.

	* include/httpd.h: Add cyg_httpd_shutdown() function to shut down
	the HTTP server.

	* src/httpd.c (HTTPD_DIAG): Update diagnostics messages.
	(cyg_httpd_shutdown): Add support for shutting the server down.

	* src/module.c: Add this file to provide support for using the
	server as a loadable module.

2008-03-03  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/httpd.c (cyg_httpd_process): Handle errors and EOF better,
	should the connection be closed prematurely.

2006-07-28  Jochen Gerster <JochenGerster@gmx.de>

	* src/monitor.c (cyg_monitor_network): Calling the network monitor
	  html handler can trigger an exception when the function
	  getifaddrs() fails because we are out of memory. Check the
	  return code and return failure if this happens.
	
2005-11-16  John Dallaway  <jld@ecoscentric.com>

	* doc/httpd.sgml: Fix typographical error.

2005-11-10  Jonathan Larmour  <jifl@eCosCentric.com>

	* doc/httpd.sgml: Fix goahead link.

2005-08-11  Nick Garnett  <nickg@ecoscentric.com>

	* tests/httpd1.c (httpd_test): Adjusted to work correctly with a
	system clock rate other than 100Hz.

2005-07-30  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/httpd.c (cyg_httpd_server): Use socklen_t to avoid compiler
	warnings.

2004-10-21  Nick Garnett  <nickg@ecoscentric.com>

	* src/httpd.c: Use CYGNUM_HAL_STACK_SIZE_TYPICAL instead of
 	CYGNUM_HAL_STACK_SIZE_MINIMUM in stacks. The minimum value is a
 	little too small when diagnostics are being sent over an ethernet
 	connection through RedBoot.

2004-10-05  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/monitor.c: include sys/sysctl.h to prevent compiler
	warnings.

2004-08-16  Peter Korsgaard <jacmet@sunsite.dk>

	* src/monitor.c: Added missing spaces in multi-line HTML strings.

2004-03-09  Nick Garnett  <nickg@calivar.com>

	* include/httpd.h: 
	* src/init.cxx: 
	* src/httpd.c: 
	* src/init.cxx:
	* doc/httpd.sgml:
	Added option to enable auto-starting of HTTPD. This is set by
	default so the current behaviour is retained. When this is
	disabled the application has to call cyg_httpd_startup() to get
	the server going.

2004-02-23  Jeff Duncan  <jeffd@magtek.com>

	* src/httpd.c (cyg_httpd_server): Fix http header by adding
          newline after server name.

2003-10-21  Eric Doenges <Eric.Doenges@DynaPel.com>

	* src/monitor.c (cyg_monitor_memory): Check if the request
	contains a 'base' parameter and don't display anything if it does
	not. This prevents the monitor from attempting to access memory
	location '0' when the user accesses the memory html page for the
	first time without any parameters.

2003-09-23  Andrew Lunn  <andrew.lunn@ascom.ch>

        * src/httpd.c (cyg_httpd_server): Removed unused variable.
        * doc/httpd.sgml: Updated documentation for previous change.

2003-09-22  Eric Doenges  <Eric.Doenges@DynaPel.com>
	
        * include/httpd.h: changed prototype of cyg_httpd_send_html and
        cyg_httpd_send_data to match implementation.

2003-06-09  Nick Garnett  <nickg@balti.calivar.com>

	* src/httpd.c: Fixed a problem with closing the client socket --
	it was being done twice.
	Tidied up the formatting a little.

	* src/monitor.c: Fixed some compiler warnings.

2003-05-11  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/monitor.c (cyg_monitor_network): Added IPv6 information to
	the display of network information.
	* tests/httpd1.c: New file: Simple program to actually run the 
	server so we can test it.
	* cdl/httpd.cdl: Added the test program.

2003-05-10  Andrew Lunn   <andrew.lunn@ascom,ch>

	* src/httpd.c: Added support for serving content over IPv6,
	* doc/httpd.sgml: Added comment about IPv6.

2003-04-23  Bob Koninckx  <bob.koninckx@mech.kuleuven.ac.be>

	* cdl/httpd.cdl: Only build monitor in CDL option.

2003-03-17  Nick Garnett  <nickg@balti.calivar.com>

	* src/monitor.c (cyg_monitor_network): Added monitoring of Mbufs
	to network page.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/httpd.cdl: Add doc link.

2003-02-14  Bob Koninckx  <bob.koninckx@mech.kuleuven.ac.be>

	* include/httpd.h (html_end): fix typo.

2002-12-06  Nick Garnett  <nickg@ecoscentric.com>

	* include/httpd.h: 
	* src/init.cxx: 
	* src/httpd.c: 
	* src/monitor.c: 
	* doc/httpd.sgml: 
	* cdl/httpd.cdl: 
	Created HTTPD package.
	
# Copyright (C) 2002 Nick Garnett
# Copyright (C) 2005 eCosCentric Limited
# All Rights Reserved.
#
# Permission is granted to use, copy, modify and redistribute this
# file.