2009-02-06  Nick Garnett  <nickg@ecoscentric.com>

	* src/malloc.cxx (MG_SET_GUARDS, MG_CHECK_GUARDS): Fix problems
	locating tail guard as a result of 2009-02-03 change.

2009-02-05  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/malloc.cxx: Fix copyright banner.

2009-09-01  Bart Veer  <bartv@ecoscentric.com>


	* src/heapgen.tcl (tcl_path): use the makefile's HOST instead of
	tcl_platform() to figure out host details.

2009-02-03  Simon Kallweit  <simon.kallweit@intefo.ch>

	* include/mvarimpl.inl:
	* include/sepmetaimpl.inl:
	Fixed a few compiler warnings.

2009-02-03  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/malloc.cxx (MG_HEAD_SIZE): Increase according to 
	CYGNUM_MEMALLOC_ALLOCATOR_DLMALLOC_ALIGNMENT if that is in use.

2009-02-03  Simon Kallweit  <simon.kallweit@intefo.ch>

	* include/mvarimpl.inl:
	* include/sepmetaimpl.inl:
	Fixed a few compiler warnings.

2009-01-09  John Dallaway  <john@dallaway.org.uk>

	* cdl/memalloc.cdl: Invoke tclsh explicitly to avoid the need for
	execute permission on heapgen.tcl.

2009-01-08  John Dallaway  <john@dallaway.org.uk>

	* src/heapgen.tcl: Specify script interpreter via /usr/bin/env.
	* cdl/memalloc.cdl: Simplify heaps.cxx make rule - cygtclsh80 is
	no-longer supported.

2008-12-19  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/dlmalloc.cxx (MALLOC_COPY): Reinstate fix of 2008-01-06
	(reverting change of 2008-11-03).
	* cdl/memalloc.cdl (CYGIMP_MEMALLOC_ALLOCATOR_DLMALLOC_USE_MEMCPY):
	Make explicit dependency on isoinfra functionality block which
	includes memmove(), and set default_value accordingly.

2008-11-03  Nick Garnett  <nickg@ecoscentric.com>

	* src/dlmalloc.cxx (MALLOC_COPY): Replace memmove() with memcpy().

	* include/dlmallocimpl.hxx (class Cyg_Mempool_dlmalloc_Implementation):
	Remove spurious typedef in definition of struct malloc_chunk.

2008-08-22  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/memalloc.cdl (CYGFUN_MEMALLOC_MALLOC_CXX_OPERATORS): 
	Adding -fexceptions is only relevant if exceptions can be supported
	as indicated by presence of libstdc++ package.
	(CYGPKG_MEMALLOC_CFLAGS_ADD): Likewise.
	* src/malloc.cxx (new, new[]): Only bother trying to throw
	exceptions if we've been built with -fexceptions.
	Fixes issue 1000594.

2008-05-22  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/sysheap.cxx: Ensure joined heap is initialised after its
	component heaps.

2008-02-19  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/malloc2.c (main): If there is insufficient heap space
	for test, make it an NA, not a failure.

2008-01-06  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/dlmalloc.cxx (MALLOC_COPY): 
	* cdl/memalloc.cdl: Use memmove instead of memcpy which can go
	wrong in realloc() when the new and old block overlaps.
	CYGIMP_MEMALLOC_ALLOCATOR_DLMALLOC_USE_MEMCPY has been retained
	instead of being renamed to ..._MEMMOVE to help backward
	compatibility with older configurations. Thanks to Oyvind Harboe
	and Dave Lawrence.

2007-11-15  Bart Veer  <bartv@ecoscentric.com>

	* host/ecosmdd: add nios2-elf to the known architectures.

2007-11-05  Oyvind Harboe <oyvind.harboe@zylin.com>
	
	* cdl/memalloc.cdl: Added option CYGBLD_MEMALLOC_MALLOC_EXTERNAL_JOIN_H
	to let applications implement a way to pick the pool to allocate memory
	from based on an application specific heuristic.
	* src/malloc.cxx: Use it.
	
2007-10-24  Oyvind Harboe <oyvind.harboe@zylin.com>
2007-10-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/malloc.cxx: Init priority for pool initialization is now
	CYG_INIT_MEMALLOC instead of before CYG_INIT_LIBC
	* src/heapgen.tcl: Ditto.

2006-09-07  Bart Veer  <bartv@ecoscentric.com>

	* cdl/memalloc.cdl: avoid compiler warnings due to unnecessary
	flags.

2006-05-17  Andrew Lunn  <andrew.lunn@ascom.ch>

	* doc/memalloc.sgml: Fix parameters for calloc. Reported by
	Andy Jackson.

2006-04-26  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/heaptest.c: CYGINT_ISO_MAIN_STARTUP needs #if.
	(main): Don't handle default constructors if it's being done
	by main() thread initialisation in CYGPKG_LIBC_STARTUP.

2006-04-11  Bart Veer  <bartv@ecoscentric.com>

	* tests/heaptest.c (main): by preference run in a thread rather
	than in cyg_start(). This facilitates testing on h/w with a
	watchdog that cannot be disabled.

2005-11-25  Jonathan Larmour  <jifl@eCosCentric.com>

	* tests/testaux.hxx: static is no longer valid for inline new.

2005-09-30  Alexander Neundorf <neundorf@kde.org>

        * doc/memalloc.sgml: two minor fixes

2005-07-30  Andrew Lunn  <andrew.lunn@ascom.ch>

	* tests/heaptest.c (test_pat): Casts to prevent compiler warnings.
	* tests/testaux.hxx: new cannot be both global and static.

2005-07-22  Andrew Lunn  <andrew.lunn@ascom.ch>

	* cdl/memalloc.cdl: Use the CXXFLAGS for the native compiler to
	avoid passing it flags only valid for C.

2005-05-10  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/memdebug.cxx: Use appropriate initialisation priority
	for heap debug support, relative to system heap.

	* src/sysheap.cxx: Use correct initialisation priorities for
	fallback and joined heaps.

2005-04-21  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/malloc.cxx (debug_alloc): Allow for the possibility of an
	invalid value being passed in which, on adding MG_HEAD_SIZE and
	MG_TAIL_SIZE causes size_t to wrap around to a slightly positive
	value. Some testsuite tests deliberately try this!
	(debug_realloc): likewise.

2005-03-27  Andrew Lunn  <andrew.lunn@ascom.ch>

	* cdl/memalloc.cdl: Added reference to documentation
	* doc/memalloc.sgml: Basic user documentation.
	* tests/heaptest.c (test_pat): Fix compiler error with 
	  diag_printf.

2005-02-18  Bart Veer  <bartv@ecoscentric.com>

	* host/ecosmdd: fix endianness issue and x86 disassembly support
	
	* host/Makefile.am, host/Makefile.in, host/acinclude.m4,
	  host/aclocal.m4, host/configure, host.configure.in:
	  implement autoconfiscation 

2005-02-07  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/heapgen.tcl: Declare pool object instances with correct
	initialization priority attribute syntax.

2005-02-02  Jonathan Larmour  <jifl@eCosCentric.com>

	* doc/memalloc.sgml: Fix minor typos.

2005-02-01  Bart Veer  <bartv@ecoscentric.com>

	* host/ecosmdd: cope with versions of Tcl < 8.4 which do not yet
	support 64-bit binary scans

2005-01-25  Bart Veer  <bartv@ecoscentric.com>

	* doc/memalloc.sgml: documentation for this package.
	
	* host/ecosmdd: new host-side tool for analyzing the debug data
	
	* src/malloc.cxx: add support for debug guards, fill-on-free, and
	separate debug data. Implement the C++ new and delete operators
	if desired.

	* cdl/memalloc.cdl: add configuration options for malloc debugging
	and the debug data. Also some general restructuring, move
	malloc.cxx to libextras.a/extras.o, and compile with -fexceptions
	if malloc.cxx provides the C++ new and delete operators.

	* src/sysheap.cxx: define the system heap if necessary. Code was
	previously in malloc.cxx, moved to a separate file for better
	linker garbage collection.

	* src/memdebug.cxx, src/memdebug.h:
	New files implementing the debug data support

	* host/mdd.gdb: new gdb script for extracting malloc debug data
	from the target.

	* src/sepmeta.cxx, src/memvar.cxx, src/memfixed.cxx, src/dlmalloc.cxx,
	  include/sepmetaimpl.inl,include/sepmetaimpl.hxx include/sepmeta.hxx,
	  include/mvarimpl.inl, include/mvarimpl.hxx, include/mfiximpl.inl,
	  include/mfiximpl.hxx, include/memvar.hxx, include/mempoolt.inl,
	  include/mempoolt.hxx, include/mempolt2.inl, include/mempolt2.hxx,
	  include/memjoin.inl, include/memjoin.hxx, include/memfixed.hxx,
	  include/dlmallocimpl.hxx, include/dlmalloc.hxx:
        Add new memory Pool function get_allocation_size()
	
2004-12-02  John Dallaway  <jld@ecoscentric.com>

	* src/malloc.cxx (cyg_memalloc_heap_reinit): Permit configurations
	with multi-region heaps to build.

2004-12-01  Nick Garnett  <nickg@ecoscentric.com>

	* src/malloc.cxx (cyg_memalloc_heap_reinit): Added this function
	to reinitialize the heap to a new arena. This should be done
	during system startup and is present mainly for the use of
	RedBoot.

2004-10-04  Oyvind Harboe  <oyvind.harboe@zylin.com>

	* src/dlmalloc.cxx (resize_alloc): No longer invoke
	 cyg_memalloc_alloc_fail() on failure to resize. It is not an out
	 of memory condition, it just means the current memory allocation
	 could not be expanded. realloc() will try allocating a completely
	 new block of memory and only if that fails do we have an out of
	 memory condition.

2004-10-01  Oyvind Harboe  <oyvind.harboe@zylin.com>

	* heapgen.tcl: place the CYGBLD_ATTRIB_INIT_PRI such that it
	compiles for gcc 3.4.2 which is more picky about its placement.

2004-06-24  Oyvind Harboe  <oyvind.harboe@zylin.com>

	* Added cyg_memalloc_alloc_fail() fn which is invoked before
	return NULL from failed allocations. Useful breakpoint site.
	Andrew Lunn wrote some of the code and pointed out various
	wrinkles to be ironed out.

2004-06-24  Oyvind Harboe  <oyvind.harboe@zylin.com>

	* Added cyg_memalloc_alloc_fail() fn which is invoked before 
	return NULL from failed allocations. Useful breakpoint site.
	Andrew Lunn wrote some of the code and pointed out various
	wrinkles to be ironed out.

2004-02-15  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/kapi.h: Add throw specifications throughout.
	* src/kapi.cxx: Ditto.

2004-02-15  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/kapi.h: Add throw specifications throughout.
	* src/kapi.cxx: Ditto.

2003-10-06  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/dlmalloc.cxx (Cyg_Mempool_dlmalloc_Implementation): Fixed
	compiler warning added by previous patch.

2003-09-30  Eric Doenges <Eric.Doengea@DynaPel.com>

	* cdl/memalloc.cdl, src/dlmalloc.cxx: Make the minimum memory
	alignment a configuration option for Doug Lea's memory allocator.

2003-02-05  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/memjoin.inl: Don't use default arg in definition.

2003-02-04  John Dallaway  <jld@ecoscentric.com>

	* src/heapgen.tcl: Accommodate POSIX-style arguments
	under Cygwin.

2003-01-29  John Dallaway  <jld@ecoscentric.com>

	* src/heapgen.tcl: Accommodate latest Cygwin Tcl shell
	(tclsh83.exe)

2002-05-10  Jonathan Larmour  <jlarmour@redhat.com>

	* tests/heaptest.c (test_pat): Make failure messages clearer.
	(cyg_start): Output what failures mean.

2002-04-24  Yoshinori Sato  <qzb04471@nifty.ne.jp>

	* src/memfixed.cxx (resize_alloc): Don't set default args in func
	definition.

2002-01-30  Bart Veer  <bartv@redhat.com>

	* tests/malloc4.cxx:
	Never call realloc() with a new size of 0, which frees the buffer.
	Fix the volatility of ptr.p

2002-01-23  Jesper Skov  <jskov@redhat.com>

	* tests/malloc4.cxx (myrand): Fix overflow.

2002-01-15  Jonathan Larmour  <jlarmour@redhat.com>

	* tests/malloc4.cxx (myrand): Fix so that it really treats the limit
	as a limit.

2001-10-17  Jesper Skov  <jskov@redhat.com>

	* include/sepmetaimpl.inl: CYGINT_ISO_STRING_MEMFUNCS checks
	changed to ifdef.

2001-10-11  Jesper Skov  <jskov@redhat.com>

	* tests/testaux.hxx (new_thread): Fixed allocation: increase
	counter before starting threads which have been allocated
	resources.

2001-10-08  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/memalloc.cdl: Only build malloc.cxx and kapi.cxx when needed.

2001-09-20  Jesper Skov  <jskov@redhat.com>

	* tests/heaptest.c: Fix failure reporting.

2001-09-07  Jesper Skov  <jskov@redhat.com>

	* tests/heaptest.c: Added some extra output on failures.

2001-08-01  Jonathan Larmour  <jlarmour@redhat.com>

	* include/sepmetaimpl.inl: Define check_free_memdq and
	check_alloced_memdq as inlines.

	* cdl/memalloc.cdl: Add new allocator supporting separate metadata,
	and the associated config options, and build sepmeta.cxx and tests.
	Build heapgeninc.tcl with macros that work with both gcc2 and gcc3.
	Ditto for heaps.o.
	Add CYGBLD_MEMALLOC_MALLOC_EXTERNAL_HEAP_H to allow external entities
	to define the heap.
	* src/malloc.cxx: Include CYGBLD_MEMALLOC_MALLOC_EXTERNAL_HEAP_H if
	defined instead of default heap definition.
	* include/sepmeta.hxx, include/sepmetaimpl.hxx, include/sepmetaimpl.inl,
	src/sepmeta.cxx, tests/sepmeta1.cxx, tests/sepmeta2.cxx:
	New files for seperated metadata allocator.

2001-07-18  Jonathan Larmour  <jlarmour@redhat.com>

	* src/heapgen.tcl: Use constructor priority of CYG_INIT_MEMALLOC
	for heap objects in generated heaps.cxx.

2001-07-12  Jonathan Larmour  <jlarmour@redhat.com>

	* tests/malloc1.c (main): Accoutn for allocators that do allocate
	space for allocs of 0.
	Test that allocating all space works.
	* src/dlmalloc.cxx (get_status): Correct again calculation of maxfree

2001-06-28  Jonathan Larmour  <jlarmour@redhat.com>

	* include/memjoin.inl (~Cyg_Mempool_Joined): free even when asserts
	disabled.

	* include/memvar.hxx (class Cyg_Mempool_Variable): Comment out argument
	names for consistency.
	* include/memfixed.hxx (class Cyg_Mempool_Fixed): Ditto.
	* include/memjoin.hxx (class Cyg_Mempool_Joined): Ditto.

2001-06-20  Jonathan Larmour  <jlarmour@redhat.com>

	* include/mvarimpl.inl (get_status): Correct calculation of maxfree
	by taking into account metadata.

2001-06-18  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/memalloc.cdl: Add heaptest test.

	* tests/heaptest.c: New test to do a memory check of all of heap.

	* src/dlmalloc.cxx (get_status): Correct maxfree and totalfree
	by accounting for block headers.

	* tests/realloc.c (cyg_start): Remove warning from declaration.
	* tests/malloc1.c (cyg_start): Ditto.
	* tests/malloc2.c (cyg_start): Ditto.
	* tests/malloc3.c (cyg_start): Ditto.
	* tests/malloc4.cxx (cyg_start): Ditto. Also add DEBUGTEST define
	and fix comment.

	* tests/testaux.hxx (STACKSIZE): Double.

2001-05-02  Hugo Tyson  <hmt@redhat.com>

	* src/dlmalloc.cxx (Cyg_Mempool_dlmalloc_Implementation): Fix
	previous change; "top" is a pseudo variable via a NULL pointer if
	the heap is not initialized, so you can't use it as a flag for "no
	mem here"; and a typo, the comparison was reversed.  The two hid
	each other, so the check for "no mem here" usually said "OK".

2001-05-01  Jonathan Larmour  <jlarmour@redhat.com>

	* include/mvarimpl.inl (try_alloc): Allow zero sized heaps.
	(Cyg_Mempool_Variable_Implementation): Ditto.
	* src/dlmalloc.cxx (try_alloc): Ditto.
	(Cyg_Mempool_dlmalloc_Implementation): Ditto.

2001-04-12  Hugo Tyson  <hmt@redhat.com>

	* include/memjoin.inl (resize_alloc): Fix typo so it compiles.
	This only applies if you configure multiple heaps.

2001-03-21  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/memalloc.cdl: Specify explicit output file when preprocessing
	heapgen.cpp. Improves portability.

2001-02-01  Jonathan Larmour  <jlarmour@redhat.com>

	* tests/malloc4.cxx: Use semaphores to sync startup order.

2000-11-28  Jonathan Larmour  <jlarmour@redhat.com>

	* src/heapgen.tcl: Don't use cygpath -s for now as not all cygwins
	have it yet.

2000-11-25  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/memalloc.cdl: Make sure PWD variable doesn't clash with bash PWD
	by renaming to XPWD

2000-11-24  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/memalloc.cdl: Invoke heapgen.tcl with build directory
	surrounded by quotes (and do so in a portable way).

	* src/heapgen.tcl: recurse back in on cygwin with correct quoting
	to allow directories containing spaces. Also in a Solaris shell
	compatible way.

2000-11-21  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/memalloc.cdl (CYGSEM_MEMALLOC_MALLOC_ZERO_RETURNS_NULL): 
	New option.
	* src/malloc.cxx (malloc): Use above option to decide if NULL should
	be returned on malloc(0).

2000-11-01  Jesper Skov  <jskov@redhat.com>

	* tests/realloc.c (main): Use reasonable factor when making too
	large realloc (targets with 64MB would cause an overflow).

2000-10-31  Jonathan Larmour  <jlarmour@redhat.com>

	* tests/testaux.hxx: Prototype cyg_hal_invoke_constructors()
	[ Forgot to check this in at the same time as below ]

2000-10-20  Jonathan Larmour  <jlarmour@redhat.com>

	* tests/dlmalloc1.cxx:
	* tests/dlmalloc2.cxx:
	* tests/malloc4.cxx:
	* tests/memfix1.cxx:
	* tests/memfix2.cxx:
	* tests/memvar1.cxx:
	* tests/memvar2.cxx:
	Make sure default priority constructors have been invoked.

2000-09-14  Jesper Skov  <jskov@redhat.com>

	* tests/realloc.c (main): fix warning.
	* tests/malloc1.c (main): Same.
	* tests/malloc2.c (main): Same.
	* tests/malloc3.c (main): Same.

2000-08-31  Jonathan Larmour  <jlarmour@redhat.com>

	* cdl/memalloc.cdl: Make dlmalloc the default malloc implementation now.
	Also add info to the variable block and dlmalloc descriptions to
	describe the pros and cons of these allocators.

2000-08-09  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* tests/malloc4.cxx (thrfree): Don't yield at loop end - actually delay
	(thrrealloc): Ditto
	(thrcalloc): Ditto
	(thrmalloc): Ditto

2000-08-08  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* tests/malloc4.cxx: Make output more frequent

2000-08-04  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* tests/dlmalloc1.cxx (STACKSIZE): Define larger than default.

2000-08-03  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* include/dlmallocimpl.hxx (class Cyg_Mempool_dlmalloc_Implementation):
	Ensure typedefs are public so dlmalloc.cxx can use them at outer level.

2000-08-02  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* src/heapgen.tcl: Fix tclsh invocation quoting problems

2000-07-31  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* src/heapgen.tcl: Allow builddir to be specified on command-line
	* cdl/memalloc.cdl: Work around NT cygtclsh80 bug by cd'ing into
	heapgen.tcl's directory before running it

2000-07-26  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* tests/malloc4.cxx: Call rand_r() rather than rand, and use a seed
	var in each thread.

2000-07-25  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* tests/malloc4.cxx (thrfree): Get mem size here. Tidy output.
	(thrmalloc): Get mem size in thrfree instead

	* src/heapgen.tcl: Refine search for user-defined name to cope with
	use of CYG_LABEL_DEFN macro

2000-07-19  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* cdl/memalloc.cdl (CYGIMP_MEMALLOC_ALLOCATOR_DLMALLOC_SAFE_MULTIPLE):
	Default to 1

	* include/mvarimpl.inl (resize_alloc): Remember to adjust other
	freelist entries when extending block

2000-07-04  Jonathan Larmour  <jlarmour@redhat.co.uk>

	* CYGPKG_MEMALLOC:

	Created as new package, merging existing memory allocator related stuff
	from the kernel and libc. Many bug fixes to existing stuff, as
	well as performance improvements, and extra features such as
	a port of dlmalloc, and the ability to support multiple disjoint
	heaps, possibly with run-time configurable size.
	There's even a bit of documentation, and some new tests

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2005, 2006, 2008 eCosCentric Limited                       
// Copyright (C) 1998, 1999, 2000, 2001, 2002 Free Software Foundation, Inc.
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================