2008-08-18  Bart Veer  <bartv@ecoscentric.com>

	* host/Makefile.am: update host-side configury
	* host/Makefile.in, host/aclocal.m4, host/configure: regenerate

2008-05-28  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/profile_gprof.cdl: This package uses mem* and str* string
	library functions, so express this in CDL.

2007-12-14  Oyvind Harboe  <oyvind.harboe@zylin.com>
2007-12-21  Jonathan Larmour  <jifl@eCosCentric.com>

	* include/profile.h: Declare profile_off.
	* src/profile.c: Added support for invoking profile_on() multiple
	times. It now stops profiling and sets up a fresh profiling range
	on every invocation using new profile_off() function.
	* doc/profile.sgml: Document it.
	
2007-10-14  Oyvind Harboe  <oyvind.harboe@zylin.com>

	* src/profile.c: do not relaunch tftpd thread upon second invocation
	of profile_on

2005-05-13  Peter Korsgaard  <jacmet@sunsite.dk>

	* doc/profile.sgml: Fixed typo in HAL support section.

2005-02-18  Bart Veer  <bartv@ecoscentric.com>

	* doc/profile.sgml, misc/gprof.gdb, host/gprof.gdb,
	  host/acinclude.m4, host/aclocal.m4, host/configure,
	  host/configure.in, host/Makefile.am, host/Makefile.in:
	  Move gprof.gdb to the host subdirectory, and autoconfiscate it.

2003-09-29  Bart Veer  <bartv@ecoscentric.com>

	* src/profile.c (profile_tftp_read_next): fix off-by-one error
	which lost the first mcount record.

	* doc/profile.sgml: fix typo

	* cdl/profile_gprof.cdl: clarify description of the tftp port

2003-09-26  Bart Veer  <bartv@ecoscentric.com>

	* cdl/profile_gprof.cdl, include/gmon.out.h, include/profile.h,
 	src/profile.c, misc/gprof.gdb, doc/gprof.sgml
	Major update, including adding call graph support.

2003-04-27  Jonathan Larmour  <jifl@eCosCentric.com>

	* src/profile.c (profile_on): Clear profile before use. Reported
	by Suzuki, Ryouzaburou.

2003-02-24  Jonathan Larmour  <jifl@eCosCentric.com>

	* cdl/profile_gprof.cdl: Add doc link.

2002-11-15  Gary Thomas  <gthomas@ecoscentric.com>

	* include/gmon_out.h: Import non-GPL version from OpenBSD.

	* doc/profile.sgml: Improve description of host/client and
	target/server roles.

	* src/profile.c: 
	* cdl/profile_gprof.cdl: Allow TFTP port number to be configured.

	* src/profile.c: 
	* include/profile.h: Add proper C++ protections.  Change timer
	callback function to be __profile_hit() - less polluting.

	* doc/profile.sgml: New file.

2002-11-14  Gary Thomas  <gthomas@ecoscentric.com>

	* src/profile.c: 
	* include/profile.h: 
	* include/gmon_out.h: 
	* cdl/profile.cdl: New package to support application profiling.

//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 2002, 2003, 2005, 2008 Free Software Foundation, Inc.      
// Copyright (C) 2003, 2005, 2008 eCosCentric Limited                       
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================