2009-04-16  Bart Veer  <bartv@ecoscentric.com>

	* ecosconfig.cxx, cdl_exec.cxx, Makefile.am, Makefile.in,
	aclocal.m4, configure: allow mingw builds

2008-08-28  Bart Veer  <bartv@ecoscentric.com>

	* configure: regenerate after update of Tcl macro

2008-08-20  Bart Veer  <bartv@ecoscentric.com>

	* configure: regenerate after update of Tcl macro

2008-08-18  Bart Veer  <bartv@ecoscentric.com>

	* Makefile.am: update host-side configury
	* Makefile.in, aclocal.m4, configure: regenerate

2008-08-15  Bart Veer  <bartv@ecoscentric.com>

	* ecosconfig.cxx, cdl_exec.cxx: avoid compiler warnings.

2006-07-10  Bart Veer  <bartv@ecoscentric.com>

	* ecosconfig.cxx: add early C++ exception throw to work around
	a cygwin issue.

2005-12-16  Bart Veer  <bartv@ecoscentric.com>

	* cdl_exec.cxx (cmd_remove): replace reserved word interface with
	iface

2005-04-05  Bart Veer  <bartv@ecoscentric.com>

	* cdl_exec.cxx (cmd_remove): check that the entities being removed
	really are packages

2003-03-26  Bart Veer  <bartv@ecoscentric.com>

	* ecosconfig.cxx: remove TRANSLATE_PATH() support, no longer
	needed and causes confusion because you end up with repositories
	containing a : character that now gets interpreted as a path
	separator. Also fix a couple of bugs related to template
	versioning.

2003-02-12  Bart Veer  <bartv@ecoscentric.com>

	* Makefile.in, configure:
	Regenerate after acinclude.m4 update

2003-02-11  Bart Veer  <bartv@ecoscentric.com>

	* ecosconfig.cxx:
	With tcl 8.4 on a windows platform it is now necessary to call
	Tcl_FindExecutable(). Otherwise Tcl does not get properly
	initialized, and can end up indirecting through a NULL function
	pointer.

2002-02-05  Bart Veer  <bartv@redhat.com>

	* cdl_exec.cxx, cdl_exec.hxx, ecosconfig.cxx:
	Add new options --enable-debug and --disable-debug

2002-01-14  Bart Veer  <bartv@redhat.com>

	* cdl_exec.cxx:
	Add missing <sys/param.h> under cygwin, needed for MAXPATHLEN.
	Reported by Jifl.

2001-12-29  Bart Veer  <bartv@redhat.com>

	* ecosconfig.cxx, cdl_exec.cxx, cdl_exec.hxx
	Add new option -n to suppress modifications to the file system,
	especially ecos.ecc. Suggested by Patrick Doyle
	(wpd@delcomsys.com)

2001-12-06  Bart Veer  <bartv@redhat.com>

	* cdl_exec.cxx (report_conflicts):
	Report possible solutions correctly (bug 56232).

2001-10-25  Julian Smart  <julians@redhat.com>

	* cdl_exec.cxx: added calls to mount -f /ecos-x under Cygwin,
    in tree command. This, along with use of /ecos-x paths in the
    makefiles, ensures that compilation is done in text mode.

2001-06-20  Bart Veer  <bartv@redhat.com>

	* cdl_exec.cxx (set_verbose_mode):
	Make the ecosconfig -v verbosity flag control libcdl database
	verbosity as well.

2001-05-16  Bart Veer  <bartv@redhat.com>

	* ecosconfig.cxx: clean up cygwin->windows path translations

	* Makefile.am: use new compiler flag support

	* configure, Makefile.in, testsuite/Makefile.in: regenerate

2001-04-27  Bart Veer  <bartv@redhat.com>

	* cdl_exec.cxx (cdl_exec::cmd_new):
	Make sure transactions get cleaned up properly if a CDL script
	fails to load.

2000-07-07  Bart Veer  <bartv@redhat.com>

	* cdl_exec.cxx (transaction_callback):
	Output the correct value irrespective of the option flavor.

2000-06-28  Bart Veer  <bartv@redhat.com>

	* cdl_exec.cxx, cdl_exec.hxx, ecosconfig.cxx:
	Fix up the reporting of conflicts, inference engine changes, etc. 

2000-04-10  Bart Veer  <bartv@redhat.com>

	* cdl_exec.cxx:
	Add diagnostic callbacks to database initialization.

2000-03-08  Bart Veer  <bartv@redhat.com>

	* configure.in (cyg_ac_infra_libdir):
	Fix typo detected by Solaris build

2000-01-20  Bart Veer  <bartv@redhat.com>

	* cdl_exec.cxx:
	Allow for libcdl interface change to CdlConfigurationBody::add()

1999-11-11  Bart Veer  <bartv@redhat.co.uk>

	* configure.in
	* configure
	* Makefile.am
	* Makefile
	Fixed VC++ build problems

1999-11-10  Bart Veer  <bartv@redhat.co.uk>

	* acinclude.m4
	* configure.in
	* Makefile.am
	* aclocal.m4
	* configure
	* Makefile.in
	Created

	* ChangeLog
	Created