Eclipse/CDT for eCos application development

John Dallaway


Introduction

Eclipse is an open-source framework and workbench for the implementation of Integrated Development Environments (IDEs). CDT is a set of additional code modules (plug-ins) for the Eclipse framework which provide C/C++ editing and debugging facilities. This document describes the process of configuring Eclipse and CDT for eCos application development. Some familiarity with Eclipse and CDT is assumed. More general user guides for the Eclipse workbench and for C/C++ development using CDT are accessible via the Help->Help Contents menu item within the Eclipse workbench.

eCosCentric provides modified versions of certain CDT plug-ins and additional plug-ins suitable for the building and debugging of eCos applications running on remote hardware using GDB. Enhancements include: