tcp_sent()
Name
tcp_sent() -- Set callback for successful transmission
Synopsis
void tcp_sent(struct tcp_pcb *pcb, err_t (*sent)
(void *arg, struct tcp_pcb *tpcb, u16_t len));
Description
Specifies the callback function that should be called when data has
successfully been received (i.e. acknowledged) by the remote
host. The len argument passed to the
sent callback function gives the
number of bytes that were acknowledged by the last acknowledgment.