netbuf_alloc()

Name

netbuf_alloc() -- Allocate space in a netbuf

Synopsis

void *netbuf_alloc(struct netbuf *buf, u16_t size);

Description

Allocates buffer memory with size number of bytes for the netbuf buf. The function returns a pointer to the allocated memory. Any memory previously allocated to the netbuf buf is deallocated. The allocated memory can later be deallocated with the netbuf_free() function. Since protocol headers are expected to precede the data when it should be sent, the function allocates memory for protocol headers as well as for the actual data.