fs mount

Name

fs mount -- Mount a filesystem

Synopsis

fs mount [-d device] {-t fstype} {mountpoint}

Arguments

NameTypeDescriptionDefault
deviceNumberDevice containing filsystem to mount.undefined
fstypeNumberFilesystem type. 
mountpointStringPathname for filesystem root./

Description

This command is used make a filesystem available for access with the filesystem access commands. Three things need to be defined to do this. First, the name of the device on which the filesystem is stored needs to be given to the -d option. Secondly, the type of filesystem it is needs to be given to the -t option. Finally, the pathname by which the new filesystem will be accessed needs to be supplied. Following a successful mount, the root of the filesystem will be accessible at the mountpoint.

Examples

Mount a JFF2 partititon:
RedBoot> fs info                                                                
Filesystems available:                                                          
ramfs                                                                           
jffs2

Devices available:
/dev/flash1

Mounted filesystems:                                                            
         Device Filesystem Mounted on                                           
    <undefined>      ramfs /
RedBoot> fs mount -d /dev/flash1 -t jffs2 /flash
RedBoot> fs info                                                                
Filesystems available:                                                          
ramfs                                                                           
jffs2

Devices available:
/dev/flash1

Mounted filesystems:                                                            
         Device Filesystem Mounted on                                           
    <undefined>      ramfs /
    /dev/flash1      jffs2 /flash
RedBoot>