fs write

Name

fs write -- Write to filesystem

Synopsis

fs write [-b mem_address] [-l length] {name}

Arguments

NameTypeDescriptionDefault
mem_addressNumberAddress of data to be written to flash.Address of last loaded file. If not set by a load operation it must be specified.
lengthNumberLength of data to be written.Length of last loaded file.
nameStringName of file to create. 

Description

This command is used to write data from memory to a file. If the file does not exist it will be created. If it does exist, then it will be overwritten with the new contents.

Examples

Write an area of data to a file
RedBoot> fs write -b 0x0606f000 -l 0x1000 image
RedBoot> fs list
212416 d---------  3 size    128 .                                              
212416 d---------  3 size    128 ..                                             
211392 ----------  1 size   4096 image                                          
206784 d---------  2 size     96 tests
RedBoot>