Some target hardware comes equipped with a watchdog timer. Application code can start this timer and after a certain period of time, typically a second, the watchdog will trigger. Usually this causes the hardware to reboot. The application can prevent this by regularly resetting the watchdog. An automatic reboot can be very useful when deploying hardware in the field: a hardware glitch could cause the unit to hang; or the software could receive an unexpected sequence of inputs, never seen in the laboratory, causing the system to lock up. Often the hardware is still functional, and a reboot sorts out the problem with only a brief interruption in service.
The synthetic target watchdog package emulates watchdog hardware. During system initialization watchdog device will be instantiated, and the watchdog.tcl script will be loaded by the I/O auxiliary. When the eCos application starts the watchdog device, the watchdog.tcl script will start checking the state of the eCos application at one second intervals. A watchdog reset call simply involves a message to the I/O auxiliary. If the watchdog.tcl script detects that a second has elapsed without a reset then it will send a SIGPWR signal to the eCos application, causing the latter to terminate. If gdb is being used to run the application, the user will get a chance to investigate what is happening. This behaviour is different from real hardware in that there is no automatic reboot, but the synthetic target is used only for development purposes, not deployment in the field: if a reboot is desired then this can be achieved very easily by using gdb commands to run another instance of the application.
Before a synthetic target eCos application can use a watchdog device it is necessary to build and install host-side support. The relevant code resides in the host subdirectory of the synthetic target watchdog package, and building it involves the standard configure, make and make install steps. The implementation of the watchdog support does not require any executables, just a Tcl script watchdog.tcl and some support files, so the make step is a no-op.
There are two main ways of building the host-side software. It is possible to build both the generic host-side software and all package-specific host-side software, including the watchdog support, in a single build tree. This involves using the configure script at the toplevel of the eCos repository. For more information on this, see the README.host file at the top of the repository. Note that if you have an existing build tree which does not include the synthetic target watchdog support then it will be necessary to rerun the toplevel configure script: the search for appropriate packages happens at configure time.
The alternative is to build just the host-side for this package. This requires a separate build directory, building directly in the source tree is disallowed. The configure options are much the same as for a build from the toplevel, and the README.host file can be consulted for more details. It is essential that the watchdog support be configured with the same --prefix option as other eCos host-side software, especially the I/O auxiliary provided by the architectural synthetic target HAL package, otherwise the I/O auxiliary will be unable to locate the watchdog support.
The watchdog device depends on the generic watchdog support, CYGPKG_IO_WATCHDOG: if the generic support is absent then the watchdog device will be inactive. Some templates include this generic package by default, but not all. If the configuration does not include the generic package then it can be added using the eCos configuration tools, for example:
$ ecosconfig add CYGPKG_IO_WATCHDOG |
By default the configuration will use the hardware-specific support, i.e. this package. However the generic watchdog package contains an alternative implementation using the kernel alarm facility, and that implementation can be selected if desired. However usually it will be better to rely on an external watchdog facility as provided by the I/O auxiliary and the watchdog.tcl script: if there are serious problems within the application, for example memory corruption, then an internal software-only implementation will not be reliable.
The watchdog resolution is currently fixed to one second: if the device does not receive a reset signal at least once a second then the watchdog will trigger and the eCos application will be terminated with a SIGPWR signal. The current implementation does not allow this resolution to be changed.
On some targets the watchdog device does not perform a hard reset. Instead the device works more or less via the interrupt subsystem, allowing application code to install action routines that will be called when the watchdog triggers. The synthetic target watchdog support effectively does perform a hard reset, by sending a SIGPWR signal to the eCos application, and there is no support for action routines.
The synthetic target watchdog package provides some configuration options for manipulating the compiler flags used for building the target-side code. That code is fairly simple, so for nearly all applications the default flags will suffice.
It should be noted that the watchdog device is subject to selective linking. Unless some code explicitly references the device, for example by calling the start and reset functions, the watchdog support will not appear in the final executable. This is desirable because a watchdog device has no effect until started.
On real hardware the watchdog device uses wallclock time: if the device does not receive a reset signal within a set period of time then the watchdog will trigger. When developing for the synthetic target this is not always appropriate. There may be other processes running, using up some or most of the cpu time. For example, the application may be written such that it will issue a reset after some calculations which are known to complete within half a second, well within the one-second resolution of the watchdog device. However if other Linux processes are running then the synthetic target application may get timesliced, and half a second of computation may take several seconds of wallclock time.
Another problem with using wallclock time is that it interferes with debugging: if the application hits a breakpoint then it is unlikely that the user will manage to restart it in less than a second, and the watchdog will not get reset in time.
To avoid these problems the synthetic target watchdog normally uses consumed cpu time rather than wallclock time. If the application is timesliced or if it is halted inside gdb then it does not consume any cpu time. The application actually has to spend a whole second's worth of cpu cycles without issuing a reset before the watchdog triggers.
However using consumed cpu time is not a perfect solution either. If
the application makes blocking system calls then it is not using cpu
time. Interaction with the I/O auxiliary involves system calls, but
these should take only a short amount of time so their effects can be
ignored. If the application makes direct system calls such as
cyg_hal_sys_read then the system behaviour
becomes undefined. In addition by default the idle thread will make
blocking select system calls, effectively waiting
until an interrupt occurs. If an application spends much of its time
idle then the watchdog device may take much longer to trigger than
expected. It may be desirable to enable the synthetic target HAL
configuration option CYGIMP_HAL_IDLE_THREAD_SPIN,
causing the idle thread to spin rather than block, at the cost of
wasted cpu cycles.
The default is to use consumed cpu time, but this can be changed in the target definition file:
synth_device watchdog {
use wallclock_time
…
} |
When the synthetic target is run in graphical mode the watchdog device extends the user interface in two ways. The Help menu is extended with an entry for the watchdog-specific documentation. There is also a graphical display of the current state of the watchdog. Initially the watchdog is asleep:
When application code starts the device the watchdog will begin to keep an eye on things (or occasionally both eyes).
If the watchdog triggers the display will change again, and optionally the user can receive an audible alert. The location of the watchdog display within the I/O auxiliary's window can be controlled via a watchdog_pack entry in the target definition file. For example the following can be used to put the watchdog display to the right of the central text window:
synth_device watchdog {
watchdog_pack -in .main.e -side top
…
} |
The user interface section of the generic synthetic target HAL documentation can be consulted for more information on window packing.
By default the watchdog support will not generate an audible alert when the watchdog triggers, to avoid annoying colleagues. Sound can be enabled in the target definition file, and two suitable files sound1.au and sound2.au are supplied as standard:
synth_device watchdog {
sound sound1.au
…
} |
An absolute path can be specified if desired:
synth_device watchdog {
sound /usr/share/emacs/site-lisp/emacspeak/sounds/default-8k/alarm.au
…
} |
Sound facilities are not built into the I/O auxiliary itself, instead an external program is used. The default player is play, a front-end to the sox application shipped with some Linux distributions. If another player should be used then this can be specified in the target definition file:
synth_device watchdog {
…
sound_player my_sound_player |
The specified program will be run in the background with a single argument, the sound file.
The watchdog support does not use any command line arguments. All configuration is handled through the target definition file.
The watchdog support does not provide any hooks for use by other scripts. There is rarely any need for customizing the system's behaviour when a watchdog triggers because those should be rare events, even during application development.