The FLASH I/O block devices can be accessed, read and written using
the standard interface supplied by the generic I/O
(CYGPKG_IO) package. These include the functions:
cyg_io_lookup() to access the device and get a
handle, cyg_io_read() and
cyg_io_write() for sequential read and write
operations, cyg_io_bread() and
cyg_io_bwrite() for random access read and write
operations, and cyg_io_get_config() and
cyg_io_setconfig() for run-time configuration
inspection and control.
However there are two aspects that differ from some other I/O devices accessed this way:
The first is that the lookup operation uses up
resources which must be subsequently freed when the last user of the
I/O handle is finished. The number of FLASH I/O devices that may be
simultaneously opened is configured with the
CYGNUM_IO_FLASH_BLOCK_DEVICES CDL option. After the
last user is finished, the device may be closed using
cyg_io_setconfig() with the
CYG_IO_SET_CONFIG_CLOSE key. Reference counting to
ensure that it is only the last user that causes a close, is left to
higher layers.
The second is that write operations assume that the flash is already erased. Attempting to write to Flash that has already been written to may result in errors. Instead FLASH must be erased before it may be written.
FLASH block devices can also be read and written using the
standard POSIX primitives, open(),
close(), read(),
write(), lseek(), and so on
if the POSIX file I/O package (CYGPKG_FILEIO) is
included in the configuration. As with the eCos generic I/O interface
you must call close() to ensure resources
are freed when the device is no longer used.
Other configuration keys are provided to perform FLASH erase
operations, and to retrieve device sizes, and FLASH block sizes at
a particular address. These operations are accessed with
cyg_io_get_config() (or if using the POSIX
file I/O API, cyg_fs_getinfo()) with the
following keys:
This erases a region of FLASH.
cyg_io_get_config() must be passed a
structure defined as per the following, which is also supplied
in <cyg/io/flash.h>:
typedef struct {
CYG_ADDRESS offset;
size_t len;
int flasherr;
cyg_flashaddr_t err_address;
} cyg_io_flash_getconfig_erase_t; |
In this structure, offset specifies
the offset within the block device to erase, len
specifies the amount to address, flasherr is
set on return to specify an error with the FLASH erase operation itself,
and err_address is used if there was an error
to specify at which address the error happened.
This protects a region of FLASH using the locking facilities
available on the card, if provided by the underlying driver.
cyg_io_get_config() must be passed a
structure defined as per the following:
typedef struct {
CYG_ADDRESS offset;
size_t len;
int flasherr;
cyg_flashaddr_t err_address;
} cyg_io_flash_getconfig_lock_t; |
In this structure, offset specifies
the offset within the block device to lock, len
specifies the amount to address, flasherr is
set on return to specify an error with the FLASH lock operation itself,
and err_address is used if there was an error
to specify at which address the error happened. If locking
support is not available -EINVAL will be returned from
cyg_io_get_config().
This disables protection for a region of FLASH using the
unlocking facilities available on the card, if provided by the underlying driver.
cyg_io_get_config() must be passed a
structure defined as per the following:
typedef struct {
CYG_ADDRESS offset;
size_t len;
int flasherr;
cyg_flashaddr_t err_address;
} cyg_io_flash_getconfig_unlock_t; |
In this structure, offset specifies
the offset within the block device to unlock, len
specifies the amount to address, flasherr is
set on return to specify an error with the FLASH unlock operation itself,
and err_address is used if there was an error
to specify at which address the error happened. If unlocking
support is not available -EINVAL will be returned from
cyg_io_get_config().
This returns the size of the FLASH block device. The
cyg_io_get_config() function must be passed a
structure defined as per the following, which is also supplied
in <cyg/io/flash.h>:
typedef struct {
size_t dev_size;
} cyg_io_flash_getconfig_devsize_t; |
In this structure, dev_size is used to
return the size of the FLASH device.
This returns the address in the virtual memory map that the
generic flash layer has been informed that this FLASH device is mapped to. Note
that some flash devices such as dataflash are not truly memory mapped,
and so this function only returns useful information when used with a true
memory mapped FLASH device. The
cyg_io_get_config() function must be passed a
structure defined as per the following, which is also supplied
in <cyg/io/flash.h>:
typedef struct {
cyg_flashaddr_t dev_addr;
} cyg_io_flash_getconfig_devaddr_t; |
In this structure, dev_addr is used to
return the address corresponding to the base of the FLASH device in the
virtual memory map.
This returns the size of a FLASH block at a
supplied offset in the FLASH block device. The
cyg_io_get_config() function must be passed a
structure defined as per the following, which is also supplied
in <cyg/io/flash.h>:
typedef struct {
CYG_ADDRESS offset;
size_t block_size;
} cyg_io_flash_getconfig_blocksize_t; |
In this structure, offset specifies the
address within the block device of which the FLASH block size is
required - a single FLASH device may contain blocks of differing
sizes. The block_size field is used to
return the block size at the specified offset.