Two different classes of serial drivers are provided as a standard part of the eCos system. These are described as “raw serial” (serial) and “tty-like” (tty).
Use the include file <cyg/io/serialio.h> for this driver.
The raw serial driver is capable of sending and receiving blocks of raw data to a serial device. Controls are provided to configure the actual hardware, but there is no manipulation of the data by this driver.
There may be many instances of this driver in a given system, one for each serial channel. Each channel corresponds to a physical device and there will typically be a device module created for this purpose. The device modules themselves are configurable, allowing specification of the actual hardware details, as well as such details as whether the channel should be buffered by the serial driver, etc.
Runtime configuration is achieved by exchanging data structures with
the driver via the cyg_io_set_config() and
cyg_io_get_config() functions.
typedef struct {
cyg_serial_baud_rate_t baud;
cyg_serial_stop_bits_t stop;
cyg_serial_parity_t parity;
cyg_serial_word_length_t word_length;
cyg_uint32 flags;
} cyg_serial_info_t; |
The field word_length contains the number of data bits per word
(character). This must be one of the values:
CYGNUM_SERIAL_WORD_LENGTH_5 CYGNUM_SERIAL_WORD_LENGTH_6 CYGNUM_SERIAL_WORD_LENGTH_7 CYGNUM_SERIAL_WORD_LENGTH_8 |
The field baud contains a baud rate selection. This must be
one of the values:
CYGNUM_SERIAL_BAUD_50 CYGNUM_SERIAL_BAUD_75 CYGNUM_SERIAL_BAUD_110 CYGNUM_SERIAL_BAUD_134_5 CYGNUM_SERIAL_BAUD_150 CYGNUM_SERIAL_BAUD_200 CYGNUM_SERIAL_BAUD_300 CYGNUM_SERIAL_BAUD_600 CYGNUM_SERIAL_BAUD_1200 CYGNUM_SERIAL_BAUD_1800 CYGNUM_SERIAL_BAUD_2400 CYGNUM_SERIAL_BAUD_3600 CYGNUM_SERIAL_BAUD_4800 CYGNUM_SERIAL_BAUD_7200 CYGNUM_SERIAL_BAUD_9600 CYGNUM_SERIAL_BAUD_14400 CYGNUM_SERIAL_BAUD_19200 CYGNUM_SERIAL_BAUD_38400 CYGNUM_SERIAL_BAUD_57600 CYGNUM_SERIAL_BAUD_115200 CYGNUM_SERIAL_BAUD_234000 |
The field stop contains the number of stop bits. This must be
one of the values:
CYGNUM_SERIAL_STOP_1 CYGNUM_SERIAL_STOP_1_5 CYGNUM_SERIAL_STOP_2 |
Note: On most hardware, a selection of 1.5 stop bits is only valid if the word (character) length is 5.
The field parity contains the parity mode. This must be one of
the values:
CYGNUM_SERIAL_PARITY_NONE CYGNUM_SERIAL_PARITY_EVEN CYGNUM_SERIAL_PARITY_ODD CYGNUM_SERIAL_PARITY_MARK CYGNUM_SERIAL_PARITY_SPACE |
The field flags is a bitmask which controls the behavior of the
serial device driver. It should be built from the values
CYG_SERIAL_FLAGS_xxx defined below:
#define CYG_SERIAL_FLAGS_RTSCTS 0x0001 |
If this bit is set then the port is placed in “hardware handshake” mode. In this mode, the CTS and RTS pins control when data is allowed to be sent/received at the port. This bit is ignored if the hardware does not support this level of handshake.
typedef struct {
cyg_int32 rx_bufsize;
cyg_int32 rx_count;
cyg_int32 tx_bufsize;
cyg_int32 tx_count;
} cyg_serial_buf_info_t; |
The field rx_bufsize contains
the total size of the incoming data buffer. This is set to zero on
devices that do not support buffering (i.e. polled devices).
The field rx_count contains the
number of bytes currently occupied in the incoming data buffer.
This is set to zero on devices that do not support buffering (i.e. polled
devices).
The field tx_bufsize contains the
total size of the transmit data buffer. This is set to zero on devices
that do not support buffering (i.e. polled devices).
The field tx_count contains the
number of bytes currently occupied in the transmit data buffer. This
is set to zero on devices that do not support buffering (i.e. polled
devices).
cyg_io_write(handle, buf, len) |
Send the data from buf to the device. The driver maintains a buffer to hold the data. The size of the intermediate buffer is configurable within the interface module. The data is not modified at all while it is being buffered. On return, *len contains the amount of characters actually consumed .
It is possible to configure the write call to be blocking
(default) or non-blocking. Non-blocking mode requires both the configuration
option CYGOPT_IO_SERIAL_SUPPORT_NONBLOCKING
to be enabled, and the specific device to be set to non-blocking
mode for writes (see cyg_io_set_config()).
In blocking mode, the call will not return until there is space in the buffer and the entire contents of buf have been consumed.
In non-blocking mode, as much as possible gets consumed from buf. If everything was consumed, the call returns ENOERR. If only part of the buf contents was consumed, -EAGAIN is returned and the caller must try again. On return, *len contains the number of characters actually consumed .
The call can also return -EINTR if interrupted
via the cyg_io_get_config()/ABORT key.
cyg_io_read(handle, buf, len) |
Receive data into the buffer, buf, from the device. No manipulation of the data is performed before being transferred. An interrupt driven interface module will support data arriving when no read is pending by buffering the data in the serial driver. Again, this buffering is completely configurable. On return, *len contains the number of characters actually received.
It is possible to configure the read call to be blocking (default)
or non-blocking. Non-blocking mode requires both the configuration
option CYGOPT_IO_SERIAL_SUPPORT_NONBLOCKING
to be enabled, and the specific device to be set to non-blocking
mode for reads (see cyg_io_set_config()).
In blocking mode, the call will not return until the requested amount of data has been read.
In non-blocking mode, data waiting in the device buffer is copied to buf, and the call returns immediately. If there was enough data in the buffer to fulfill the request, ENOERR is returned. If only part of the request could be fulfilled, -EAGAIN is returned and the caller must try again. On return, *len contains the number of characters actually received.
The call can also return -EINTR if interrupted via
the cyg_io_get_config()/ABORT
key.
cyg_io_get_config(handle, key, buf, len) |
This function returns current [runtime] information about the device and/or driver.
cyg_serial_info_t
This function retrieves the current state of the driver and hardware. This information contains fields for hardware baud rate, number of stop bits, and parity mode. It also includes a set of flags that control the port, such as hardware flow control.
cyg_serial_buf_info_t
This function retrieves the current state of the software buffers in the serial drivers. For both receive and transmit buffers it returns the total buffer size and the current number of bytes occupied in the buffer. It does not take into account any buffering such as FIFOs or holding registers that the serial device itself may have.
void *
This function waits for any buffered output to complete. This function only completes when there is no more data remaining to be sent to the device.
void *
This function discards any buffered output for the device.
void *
This function discards any buffered input for the device.
void*
This function will cause any pending read or write calls on this device to return with -EABORT.
cyg_uint32 (values 0 or 1)
This function will read back the blocking-mode setting for read calls on this device. This call is only available if the configuration option CYGOPT_IO_SERIAL_SUPPORT_NONBLOCKING is enabled.
cyg_uint32 (values 0 or 1)
This function will read back the blocking-mode setting for write calls on this device. This call is only available if the configuration option CYGOPT_IO_SERIAL_SUPPORT_NONBLOCKING is enabled.
cyg_io_set_config(handle, key, buf,len) |
This function is used to update or change runtime configuration of a port.
cyg_serial_info_t
This function updates the information for the driver and hardware. The information contains fields for hardware baud rate, number of stop bits, and parity mode. It also includes a set of flags that control the port, such as hardware flow control.
cyg_uint32 (values 0 or 1)
This function will set the blocking-mode for read calls on this device. This call is only available if the configuration option CYGOPT_IO_SERIAL_SUPPORT_NONBLOCKING is enabled.
cyg_uint32 (values 0 or 1)
This function will set the blocking-mode for write calls on this device. This call is only available if the configuration option CYGOPT_IO_SERIAL_SUPPORT_NONBLOCKING is enabled.