#include <cyg/kernel/kapi.h>
|
void cyg_mbox_create(cyg_handle_t* handle, cyg_mbox* mbox);
void cyg_mbox_delete(cyg_handle_t mbox);
void* cyg_mbox_get(cyg_handle_t mbox);
void* cyg_mbox_timed_get(cyg_handle_t mbox, cyg_tick_count_t abstime);
void* cyg_mbox_tryget(cyg_handle_t mbox);
cyg_count32 cyg_mbox_peek(cyg_handle_t mbox);
void* cyg_mbox_peek_item(cyg_handle_t mbox);
cyg_bool_t cyg_mbox_put(cyg_handle_t mbox, void* item);
cyg_bool_t cyg_mbox_timed_put(cyg_handle_t mbox, void* item, cyg_tick_count_t abstime);
cyg_bool_t cyg_mbox_tryput(cyg_handle_t mbox, void* item);
cyg_bool_t cyg_mbox_waiting_to_get(cyg_handle_t mbox);
cyg_bool_t cyg_mbox_waiting_to_put(cyg_handle_t mbox);
Mail boxes are a synchronization primitive. Like semaphores they can be used by a consumer thread to wait until a certain event has occurred, but the producer also has the ability to transmit some data along with each event. This data, the message, is normally a pointer to some data structure. It is stored in the mail box itself, so the producer thread that generates the event and provides the data usually does not have to block until some consumer thread is ready to receive the event. However a mail box will only have a finite capacity, typically ten slots. Even if the system is balanced and events are typically consumed at least as fast as they are generated, a burst of events can cause the mail box to fill up and the generating thread will block until space is available again. This behaviour is very different from semaphores, where it is only necessary to maintain a counter and hence an overflow is unlikely.
Before a mail box can be used it must be created with a call to
cyg_mbox_create. Each mail box has a unique
handle which will be returned via the first argument and which should
be used for subsequent operations.
cyg_mbox_create also requires an area of memory
for the kernel structure, which is provided by the
cyg_mbox second argument. If a mail box is
no longer required then cyg_mbox_delete can be
used. This will simply discard any messages that remain posted.
The main function for waiting on a mail box is
cyg_mbox_get. If there is a pending message
because of a call to cyg_mbox_put then
cyg_mbox_get will return immediately with the
message that was put into the mail box. Otherwise this function
will block until there is a put operation. Exceptionally the thread
can instead be unblocked by a call to
cyg_thread_release, in which case
cyg_mbox_get will return a null pointer. It is
assumed that there will never be a call to
cyg_mbox_put with a null pointer, because it
would not be possible to distinguish between that and a release
operation. Messages are always retrieved in the order in which they
were put into the mail box, and there is no support for messages
with different priorities.
There are two variants of cyg_mbox_get. The
first, cyg_mbox_timed_get will wait until either
a message is available or until a number of clock ticks have occurred.
The number of ticks is specified as an absolute, not relative tick
count, and so in order to wait for a relative number of ticks, the
return value of the cyg_current_time() function
should be added to determine the absolute number of ticks. If no
message is posted within the timeout then a null pointer will be
returned. cyg_mbox_tryget is a non-blocking
operation which will either return a message if one is available or a
null pointer.
New messages are placed in the mail box by calling
cyg_mbox_put or one of its variants. The main put
function takes two arguments, a handle to the mail box and a
pointer for the message itself. If there is a spare slot in the
mail box then the new message can be placed there immediately, and
if there is a waiting thread it will be woken up so that it can
receive the message. If the mail box is currently full then
cyg_mbox_put will block until there has been a
get operation and a slot is available. The
cyg_mbox_timed_put variant imposes a time limit
on the put operation, returning false if the operation cannot be
completed within the specified number of clock ticks and as for
cyg_mbox_timed_get this is an absolute tick
count. The cyg_mbox_tryput variant is
non-blocking, returning false if there are no free slots available and
the message cannot be posted without blocking.
There are a further four functions available for examining the current
state of a mailbox. The results of these functions must be used with
care because usually the state can change at any time as a result of
activity within other threads, but they may prove occasionally useful
during debugging or in special situations.
cyg_mbox_peek returns a count of the number of
messages currently stored in the mail box.
cyg_mbox_peek_item retrieves the first message,
but it remains in the mail box until a get operation is performed.
cyg_mbox_waiting_to_get and
cyg_mbox_waiting_to_put indicate whether or not
there are currently threads blocked in a get or a put operation on a
given mail box.
The number of slots in each mail box is controlled by a configuration option CYGNUM_KERNEL_SYNCH_MBOX_QUEUE_SIZE, with a default value of 10. All mail boxes are the same size.
cyg_mbox_create is typically called during
system initialization but may also be called in thread context.
The remaining functions are normally called only during thread
context. Of special note is cyg_mbox_put which
can be a blocking operation when the mail box is full, and which
therefore must never be called from DSR context. It is permitted to
call cyg_mbox_tryput,
cyg_mbox_tryget, and the information functions
from DSR context but this is rarely useful.