#include <stdlib.h>
#include <new>
|
void* malloc(size_t size);
void* calloc(size_t nmemb, size_t size);
void* realloc(void* ptr, size_t size);
void free(void* ptr);
struct mallinfo mallinfo(void);
void* operator new(size_t size);
void* operator new[](size_t size);
void* operator new(size_t size, const std::nothrow_t&);
void* operator new(nothrow)[](size_t size, const std::nothrow_t&);
void operator delete(void* ptr);
void operator delete[](void* ptr);
void operator delete(void* ptr, const std::nothrow_t&);
void operator delete[](void* ptr, const std::nothrow_t&);
The dynamic memory allocation package
CYGPKG_MEMALLOC provides support for the ISO
standard C functions malloc,
calloc, realloc and
free. Optionally it can provide the C++
new and delete operators.
There is extensive support for debugging various problems associated
with dynamic memory allocation.
Some of the available target RAM will be needed for application code and static data. If the target uses RedBoot or another ROM monitor for bootstrap then that may also reserve some of the available RAM. On most targets the system heap occupies all remaining RAM, and this is used to satisfy the memory allocation requests. By default the Doug Lea memory allocator (dlmalloc) code is used to manage the heap. This provides a good trade off between efficient use of the memory, fast operation, and resistance to fragmentation. If the eCos configuration includes the kernel then by default the various memory allocation routines will be thread-safe.
To complement the standard APIs the memory allocation package provides support for custom memory pools.
The main dynamic memory allocation routines defined by standard C is
malloc(): this allocates a chunk of memory from
the heap at least as large as the amount requested, satisfying any
alignment restrictions imposed by the architecture. The initial
contents of the allocated chunk is undefined. If the heap cannot
satisfy the allocation request then a null pointer will be returned.
The standard does not define what happens when
malloc() is passed a size of 0. In eCos this is
controlled by a configuration option
CYGSEM_MEMALLOC_MALLOC_ZERO_RETURNS_NULL. By
default the option is disabled and an argument of
0 will still result in an allocation of
the smallest size supported by the memory allocator. If the option is
enabled then a null pointer will be returned instead.
calloc() tries to allocate a memory chunk of at
least nmemb*size bytes. If the allocation succeeds
then the memory will be filled with zeroes. Otherwise a null pointer
is returned.
realloc() tries to change the size of an existing
allocation while leaving the contents unchanged. This may involve resizing the
chunk in situ, or it may involve a
malloc()/memcpy()/free()
sequence. If the operation succeeds a valid pointer will be returned,
which may or may not be the same as the original pointer. If the
operation fails then a null pointer will be returned and the original
data remains intact. There are two special cases: if the
ptr argument is a null pointer then
realloc() will act like
malloc(); otherwise if the
size argument is 0 then
realloc() will act like
free().
free() takes a pointer previously returned by
malloc(), calloc() or
realloc() and returns the memory to the heap.
mallinfo() is not defined by the C standard but
is provided for compatibility with other systems. It returns
information about the current state of the heap in the form of a
mallinfo structure:
struct mallinfo {
int arena; /* total size of memory arena */
int ordblks; /* number of ordinary memory blocks */
int uordblks; /* space used by ordinary memory blocks */
int fordblks; /* space free for ordinary blocks */
int maxfree; /* size of largest free block */
};
|
arena gives the total heap size.
ordblks and
uordblks give some information on current
allocations, and fordblks indicates how
much is left. The remaining memory may be fragmented so
maxfree indicates the largest allocation
that is currently possible. A mallinfo
structure contains a number of other fields but those are not used by
eCos and exist only for compatibility reasons.
C++ applications can use the standard C library routines for dynamic
memory allocation, but it is more common to use the C++
new and delete operators.
There are a number of different implementations of these:
The infrastructure package contains empty versions of the delete
operators which do not interact with the system heap in any way. This
is necessary because of the way the g++ compiler
handles certain language constructs. Whenever there is a class with a
virtual destructor the generated code always contains a reference to
the delete operator. The linker is unable to
delete this. Therefore if the application uses such a class, directly
or indirectly, the final executable will contain a
delete implementation - even if there is no
dynamic allocation. The usual delete operator
would pull in the system heap and hence the memory allocation package,
significantly increasing code size for no good reason. Providing an
empty delete avoids this.
Unfortunately this solution is imperfect. If instead the application
does want to create and destroy objects on the heap, by default the
empty delete operators will still get linked in
and the memory never gets freed. It is not possible to handle both
scenarios cleanly with current tools, so instead the application
developer has to configure eCos appropriately. To suppress the empty
delete operators the configuration option
CYGFUN_INFRA_EMPTY_DELETE_FUNCTIONS should be
disabled. If an eCos package performs dynamic memory allocation using
C++ new and delete then it
should automatically disable this option via a CDL
requires property.
The next implementation of new and
delete comes in the C++ support library
libsupc++.a, which is normally available as part
of the GNU toolchain. These versions are straightforward, simply
calling malloc() and free()
to access the system heap. When linking an application with an eCos
linker script the C++ support library is searched automatically, so
application developers only need to worry about disabling
CYGFUN_INFRA_EMPTY_DELETE_FUNCTIONS.
Finally the memory allocation package can also provide implementations
of the C++ operators. These access the system heap directly rather
than going via malloc() and
free() so can be marginally faster, but at the
cost of some increased code size. There is a significant difference of
the system is configured for collecting memory debug data. These
implementations of new and
delete integrate directly with the debug data
code, so more information will be collected. This is especially
useful on architectures where the compiler only provides limited
backtrace support.
The configuration option CYGFUN_MEMALLOC_MALLOC_CXX_OPERATORS controls whether or not the memory allocation package's versions of the C++ operators get built. By default this option is disabled, unless CYGDBG_MEMALLOC_DEBUG_DEBUGDATA is enabled. When linking an application with an eCos linker script these operators will automatically be used in preference to the ones in libsupc++.a.
An application that uses dynamic memory allocation is often more difficult to debug than one that relies entirely on static allocation. To assist developers the memory allocation package provides a number of debugging facilities. The main one involves the collection of additional debug data for every memory allocation. This debug data can be transferred to the host and analyzed using a custom tool ecosmdd. Full documentation on this is provided elsewhere.
This package also provides support for some simple debugging
techniques which can help detect certain problems. The first is memory
guards: every allocated chunk is surrounded by a number of guard
bytes. When the chunk is freed, using free() or
the appropriate C++ delete operator, the guards
are checked and any discrepancy is treated as an assertion failure.
The head guard can detect certain buffer overflows in the previously
allocated chunk. If the chunk contains a thread stack and the
architecture involves a descending stack then the head guard can also
detect stack overflows. The tail guard can detect certain overflows in
the chunk being freed and underflows in the next chunk. The guards are
reset during a free operation, which can help to catch attempts to
free the same chunk twice. Guard checks only happen during a free
operation so a corruption may go undetected for a long time, possibly
too long, but are still better to never detecting corruption.
Memory guards are controlled by the configuration option CYGDBG_MEMALLOC_MALLOC_DEBUG_GUARDS. By default they are enabled if system-wide debugging (CYGPKG_INFRA_DEBUG) is enabled, otherwise disabled.
The second debugging technique is to fill memory chunks when they are freed. This helps to catch some attempts to use a pointer which is no longer valid. Such problems are particularly common in multi-threaded applications where thread A frees a chunk that thread B is still using. When freed chunks are filled thread B will suddenly see spurious data, often resulting in bus errors or other exceptions. The relevant configuration option is CYGDBG_MEMALLOC_MALLOC_DEBUG_FILL_FREE, which by default is also enabled if CYGPKG_INFRA_DEBUG is enabled. The option's value determines what the freed chunk gets filled with, usually 0xff.