Chapter 52. SNMP for eCos

Table of Contents
Version
SNMP packages in the eCos source repository
MIBs supported
Changes to eCos sources
Starting the SNMP Agent
Configuring eCos
Test cases
SNMP clients and package use
Unimplemented features
MIB Compiler
snmpd.conf

Version

This is a port of UCD-SNMP-4.1.2

Originally this document said: See http://ucd-snmp.ucdavis.edu/ for details. And send them a postcard.

The project has since been renamed “net-snmp” and re-homed at http://net-snmp.sourceforge.net/ where various new releases (of the original, not eCos ports) are available.

The original source base from which we worked to create the eCos port is available from various archive sites such as ftp://ftp.freesnmp.com/mirrors/net-snmp/ generally with this filename and details:
ucd-snmp-4.1.2.tar.gz. . . . . . Nov  2  2000   1164k