Before going into detail, let's look at a simple example of how the eCos PPP package is used. Consider the following example:
static void ppp_up(void)
{
cyg_ppp_options_t options;
cyg_ppp_handle_t ppp_handle;
// Bring up the TCP/IP network
init_all_network_interfaces();
// Initialize the options
cyg_ppp_options_init( &options );
// Start up PPP
ppp_handle = cyg_ppp_up( "/dev/ser0", &options );
// Wait for it to get running
if( cyg_ppp_wait_up( ppp_handle ) == 0 )
{
// Make use of PPP
use_ppp();
// Bring PPP link down
cyg_ppp_down( ppp_handle );
// Wait for connection to go down.
cyg_ppp_wait_down( ppp_handle );
}
} |
This is a simple example of how to bring up a simple PPP connection to another computer over a directly connected serial line. The other end is assumed to already be running PPP on the line and waiting for a connection.
The first thing this code does is to call
init_all_network_interfaces() to bring up the
TCP/IP stack and initialize any other network interfaces. It then
calls cyg_ppp_options_init() to initialize the
PPP options structure to the defaults. As it happens, the default
options are exactly what we want for this example, so we don't need to
make any further changes. We go straight on to bring the PPP interface
up by calling cyg_ppp_up(). The arguments to this
function give the name of the serial device to use, in this case
"/dev/ser0", and a pointer to the options.
When cyg_ppp_up() returns, it passes back a
handle to the PPP connection which is to be used in other calls. The
PPP link will not necessarily have been fully initialized at this
time. There is a certain amount of negotiation that goes on between
the ends of a PPP link before it is ready to pass packets. An
application can wait until the link is ready by calling
cyg_ppp_wait_up(), which returns
zero if the link is up and running, or
-1 if it has gone down or failed to come up.
After a successful return from cyg_ppp_wait_up(),
the application may make use of the PPP connection. This is
represented here by the call to use_ppp() but
it may, of course, be accessed by any thread. While the connection is
up the application may use the standard socket calls to make or accept
network connections and transfer data in the normal way.
Once the application has finished with the PPP link, it can bring it
down by calling cyg_ppp_down(). As with bringing
the connection up, this call is asynchronous, it simply informs the
PPP subsystem to start bringing the link down. The application can
wait for the link to go down fully by calling
cyg_ppp_wait_down().
That example showed how to use PPP to connect to a local peer. PPP is more often used to connect via a modem to a remote server, such as an ISP. The following example shows how this works:
static char *isp_script[] =
{
"ABORT" , "BUSY" ,
"ABORT" , "NO CARRIER" ,
"ABORT" , "ERROR" ,
"" , "ATZ" ,
"OK" , "AT S7=45 S0=0 L1 V1 X4 &C1 E1 Q0" ,
"OK" , "ATD" CYGPKG_PPP_DEFAULT_DIALUP_NUMBER ,
"ogin:--ogin:" , CYGPKG_PPP_AUTH_DEFAULT_USER ,
"assword:" , CYGPKG_PPP_AUTH_DEFAULT_PASSWD ,
"otocol:" , "ppp" ,
"HELLO" , "\\c" ,
0
};
static void ppp_up(void)
{
cyg_ppp_options_t options;
cyg_ppp_handle_t ppp_handle;
// Bring up the TCP/IP network
init_all_network_interfaces();
// Initialize the options
cyg_ppp_options_init( &options );
options.script = isp_script;
options.modem = 1;
// Start up PPP
ppp_handle = cyg_ppp_up( "/dev/ser0", &options );
// Wait for it to get running
if( cyg_ppp_wait_up( ppp_handle ) == 0 )
{
// Make use of PPP
use_ppp();
// Bring PPP link down
cyg_ppp_down( ppp_handle );
// Wait for connection to go down.
cyg_ppp_wait_down( ppp_handle );
}
} |
The majority of this code is exactly the same as the previous
example. The main difference is in the setting of a couple of options
before calling cyg_ppp_up(). The
script option is set to point to a CHAT
script to manage the setup of the connection. The
modem option is set to cause the PPP system
to make use of the modem control lines.
During the PPP bring-up a call will be made to
cyg_ppp_chat() to run the CHAT script (see Chapter 47). In the example this script sets up various modem
options and then dials a number supplied as part of the PPP package
configuration (see Chapter 46). When the connection
has been established, the script log on to the server, using a name
and password also supplied by the configuration, and then starts PPP
on the remote end. If this script succeeds the PPP connection will be
brought up and will then function as expected.
The modem option causes the PPP system to
make use of the modem control lines. In particular it waits for
Carrier Detect to be asserted, and will bring the
link down if it is lost. See cyg_ppp_options_init()
for more details.