2004-10-21  Nick Garnett  <nickg@ecoscentric.com>

	* src/if_i82544.c (i82544_can_send): Removed calls to
	PacketRxReady() and TxDone(). These can result in recursive calls
	back into the driver, which may use up too much stack.

2004-09-10  Nick Garnett  <nickg@ecoscentric.com>

	* src/if_i82544.c (i82544_setup): Changed return values of
	i82544_setup() and i82544_init() to detect failure of the link to
	come up and return false. In RedBoot this short circuits many of
	the startup delays when the ethernet is not plugged in.

2004-05-14  Nick Garnett  <nickg@ecoscentric.com>

	* src/if_i82544.c (i82544_setup, i82544_poll) 
	(pci_init_find_82544s): Fixed interrupt enable, masking
	and acknowledges so that the driver correctly handles Ctrl-C
	interrupts in RedBoot.
	(i82544_can_send): Added test for recursion here, and return zero
	in inner calls.

2003-01-17  Andrew Lunn	 <andrew.lunn@ascom.ch>

	* src/if_i82544.c: Fixed a few compiler warnings.
	
2004-01-15  Kevin Lemay  <kevin.lemay@agilent.com>

	* src/if_i82544.c: Added support for the i82540 device. 

2003-05-16  Mark Salter  <msalter@redhat.com>

	* include/i82544_info.h: Add link flag.
	* src/if_i82544.c: Allow booting when not using ASD and link is down.

2003-03-19  Mark Salter  <msalter@redhat.com>

	* src/if_i82544.c (i82544_setup): More 82546 EEPROM fixes (EE_PRES
	appears to be unreliable).

2003-03-17  Mark Salter  <msalter@redhat.com>

	* src/if_i82544.c: Fix 82546 EEPROM access. Fix ESA address for second
	port of 82546.

2003-03-11  Mark Salter  <msalter@redhat.com>

	* src/if_i82544.c (find_82544s_match_func): Add 82546 devid.

2003-02-05  Nick Garnett  <nickg@calivar.com>

	* src/if_i82544.c (BUS_TO_VIRT): Added default definition of this
	macro.

2002-11-12  Gary Thomas  <gary@mlbassoc.com>

	* src/if_i82544.c: Minor fixes - use HAL_DELAY_US(), additional
	PCI device type (0x100D) which is present on the NPWR Linux Engine.

2002-06-14  Gary Thomas  <gary@chez-thomas.org>

	* src/if_i82544.c: 
	Need to include <pkgconf/io_eth_drivers.h> for proper configuration
	of stand-alone (polled) vs. system (interrupt driven) mode.

2002-02-25  Mark Salter  <msalter@redhat.com>

	* src/if_i82544.c: Don't call PacketRxReady in standalone configuration
	unless ready to accept a packet. Limit packet delivery to one packet at
	a time in standalone configuration.

2002-02-22  Mark Salter  <msalter@redhat.com>

	* src/if_i82544.c: Remove unnecessary eth_dsr declaration.

2002-02-19  Mark Salter  <msalter@redhat.com>

	* src/if_i82544.c (pci_init_find_82544s): Don't use IRQ support if
	CYGPKG_IO_ETH_DRIVERS_STAND_ALONE.

2002-01-22  Mark Salter  <msalter@redhat.com>

	* src/if_i82544.c (i82544_send): Add HAL_DCACHE_STORE before passing
	buffer to NIC.

2002-01-21  Mark Salter  <msalter@redhat.com>

	* cdl/intel_i82544_eth_drivers.cdl: Add
	CYGNUM_DEVS_ETH_INTEL_I82544_MAX_RX_DESCRIPTORS and
	CYGNUM_DEVS_ETH_INTEL_I82544_MAX_TX_DESCRIPTORS.

	* src/if_i82544.c: Add appropriate BUS_TO_VIRT and VIRT_TO_BUS
	conversions.
	Remove check that assumes driver owns entire PCI window.
	(i82544_setup): Add option to use auto-speed detection.

2001-11-27  Nick Garnett  <nickg@redhat.com>

	* cdl/intel_i82544_eth_drivers.cdl: 
	* include/i82544_info.h: 
	* src/if_i82544.c: 
	Created driver by copying i82559 driver and editing.
	
//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004 Free Software Foundation, Inc.
// Copyright (C) 2004 eCosCentric Limited                                   
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================