2007-05-30  Hajime Ishitani <pigmon@mail.snd.co.jp>

	* src/if_8139.c:
	* cdl/rltk_8139_eth_drivers.cdl
	add write in MAC address at EEPROM by SIOCSIFHWADDR.

2006-12-17  Hajime Ishitani <pigmon@mail.snd.co.jp>

	* src/if_8139.c:
	added 0x10ec/0x8129 for RTL8139C(L) of a known device.

2006-11-13  Hajime Ishitani <pigmon@mail.snd.co.jp>

	* src/if_8139.c: Enabled "PUN/LinkChg" interrupt.

2005-12-02  Andrew Lunn  <andrew.lunn@ascom.ch>

	* src/if_8139.c (rltk8139_deliver): Fix the compiler warnings by
	adding some casts.

2005-11-25  Hajime Ishitani <pigmon@mail.snd.co.jp>

	* src/if_8139.h:
	* src/if_8139.c: Added a priority level field

2005-03-03  Bob Koninckx <bob.koninckx@fmtc.be>

	* src/if_8139.c: fixed bug that prevented rltk8139_find to find
	anything but first device.

2004-10-18  Andrew Dyer  <adyer@righthandtech.com>

	* src/if_8139.c (rltk8139_recv): if eth_drv_recv() wants to
	discard an incoming packet it sets the buffer address == 0. Add a
	check for this and skip the memcpy if found.

2004-05-17  John Dallaway  <jld@ecoscentric.com>

	* src/if_8139.c: Add further PCI vendor/device codes (untested).

2004-05-14  Nick Garnett  <nickg@ecoscentric.com>

	* src/if_8139.c: Fixed interrupt enable, masking and acknowledges
	so that the driver correctly handles Ctrl-C interrupts in RedBoot.

2004-05-13  Nick Garnett  <nickg@ecoscentric.com>

	* src/if_8139.c (rltk8139_find): Don't reinitialize pci_device_id
	each time around the loop.
	(rltk8139_recv): Avoid copying data when passed a NULL
	buffer. This can happen if the stack runs out of MBUFs.

2004-05-11  John Dallaway  <jld@ecoscentric.com>

	* src/if_8139.c: Add D-Link DFE-538TX rev E1 vendor/device codes.

2004-04-21  Yoshinori Sato <ysato@users.sourceforge.jp>

	* src/if_8139.c:
	add known device 0x11db/0x1234 from Dreamcast Broadband Adapter.
	add Platform depend Initialize entry.

2003-11-21  Gary Thomas  <gary@mlbassoc.com>

	* src/if_8139.c: Use cyg_drv_isr_lock/unlock functions for ISR
	critical sections - much better than calling cyg_interrupt_enable
	directly.

2003-07-09  Eric Doenges <Eric.Doenges@DynaPel.com>

	* src/if_8139.h: 
	* src/if_8139.c: 
	* doc/README: 
	* cdl/rltk_8139_eth_drivers.cdl: 
	New package - PCI ethernet driver for RTL8139 cards,
	(using the Intel 82259 driver as inspiration).
	
//===========================================================================
// ####GPLCOPYRIGHTBEGIN####                                                
// -------------------------------------------                              
// This file is part of eCos, the Embedded Configurable Operating System.   
// Copyright (C) 1998, 1999, 2000, 2001, 2002, 2004 Free Software Foundation, Inc.
// Copyright (C) 2004 eCosCentric Limited                                   
//
// This program is free software; you can redistribute it and/or modify     
// it under the terms of the GNU General Public License as published by     
// the Free Software Foundation; either version 2 or (at your option) any   
// later version.                                                           
//
// This program is distributed in the hope that it will be useful, but      
// WITHOUT ANY WARRANTY; without even the implied warranty of               
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU        
// General Public License for more details.                                 
//
// You should have received a copy of the GNU General Public License        
// along with this program; if not, write to the                            
// Free Software Foundation, Inc., 51 Franklin Street,                      
// Fifth Floor, Boston, MA  02110-1301, USA.                                
// -------------------------------------------                              
// ####GPLCOPYRIGHTEND####                                                  
//===========================================================================